Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51187 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

    Do you know of any library that contains castellations for PCB's ?      I am making a surface mount PCB that contains castellated edges for pads and wanted to check to see if they exist  before I make them myself.

     

    Thanks,

    Joe A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joe,

     

    I am sorry, but I am not familiar with the expression "Castellated edges". Is this something like passer marks which we have in our marks.lbr?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • igalloway
    igalloway over 14 years ago in reply to Richard_H

    Castillated edges could be two things...

    - series of (unplated) drill holes closely spaced  in a row so that

    the board breaks off there.

    -  I/O signals and power for the entire board are routed the

    equivalent of large vias (plated drill holes) cut in half right at the

    edge of the board, that are then used to make the board like a

    "surface mount" assembly. Sometimes found on things like a smt radio

    module.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • igalloway
    igalloway over 14 years ago in reply to Richard_H

    Castillated edges could be two things...

    - series of (unplated) drill holes closely spaced  in a row so that

    the board breaks off there.

    -  I/O signals and power for the entire board are routed the

    equivalent of large vias (plated drill holes) cut in half right at the

    edge of the board, that are then used to make the board like a

    "surface mount" assembly. Sometimes found on things like a smt radio

    module.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joe,

     

    you can use two pads as well. Best would be then to use two pins and connect them both with the signal....

    Currently there is no better solution. We have to wait for EAGLE version 6. There we will have the possibility to connect one pin to several pads and it will be possible to draw arbitrary pad shapes with a POLYGON or WIREs. There won't be DRC errors and polygons in the layout will be connected or isolated properly.

     

    Best regards,

    Richard

     

    BTW: You know that "Adler" is the German word for "eagle"?  SCNR...  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Richard,

    Thanks for the quick reply.

    I find that when I make the library part, if I just add another square pad to cover one round end of the test point pad, I wind up with the shape I need wiithout having to draw any polygons.

    The stop layer is made automatically and shows up on the PCB when I enable the layer to see it.

    The only problem I still have is that when I connect the PAD to ground and pour a ground plane, the section of the PAD that is made by the square does not connect to ground.  The other part of the pad (the part with the two rounded ends) connects just fine.

    I was thinking of making another PAD that would have a separate connection for both pads and I would just connect both to ground on the schematic.

    I hope this makes sense.  Anyway, thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joe,

     

    the way you did it is okay. You have to use an SMD and use for example a polygon to create the final shape. please think of solder stop maks and solder paste. You have to draw this in layers tStop and tCream manually. You will get an DRC error in the layout editor which you have to approve.

    Be sure that the polygon does not use a too fine wire width.  So there won't be any problems with manufacturing your board.

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Thanks for your help with this.  It turns out to be an easy thing to accomplish.

    I have one more question.

    Is there any way to make an SMD pad that is shaped like a rectangle, but has a square end on one side and a rounded end on the other side?

    What I do right now is to add a square SMD pad at the end of the SMD pad that is rounded at both ends. I dont connect it to anything when I make the device.

    I used this method to make a new test pad library part.

    This works fine, but I am not sure if this will cause any problems down the road.

    What do you think?  Is there a better way to do this?

    Thanks again,

    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • igalloway
    igalloway over 14 years ago in reply to Richard_H

    BTW - I tried it once (Case 2) , - exactly as you mentioned (just put

    plated vias at edge of board) and have mfr mill through them, and the

    castellated pads seem very fragile. Of course this is dependent on the

    manufacturer etc....

     

    At the time i also was wondering if there was a "bettter way".

    Ideallly the plating-up needs to happen AFTER a milling operation during

    manufacturing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to igalloway

    Hi Iain,

     

    thank you very much for your explanation.... image 

     

    @all and @Joe: There are no such objects in our libraries. You have to create them by yourself.

    But this can be done very easily: Choose a decent grid and place HOLEs. This can be done in the libara editor or in the layout dierctly.

     

    For the second possibility Iain mentioned, you have to take vias and place them at the edge of the board. In the manufacturing process the vias will be cut into half when milling the board contour.

     

    Regards,

    Richard