Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51166 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

    Thanks for all the helps so far, you've been great. I have problem with Eagle and I'm stumped to find an answer. Before I send our boards out I prototype them here. Because we can't do certain operations like running the top layer to thru hole capacitors we need to stop the auto router from running the top layer to those locations. We have been using the restrict layer to keep the top tracks from those locations but this is tedious on larger boards. Is there a simple way we can limit track layers to certain packages? Maybe when 6 comes out if not now?

     

    Thanks,

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Richard,

     

    Thanks to your help my project is almost ready to send to the fab house.

     

    One problem I'm having is that the drc returns overlap errors everywhere I use rectangles.  I also have the problem of connecting signals of different names (sub grounds) to one point - it returns overlap errors.  Is there any way to give a rectangle a name or otherwise make it a part of a network so the drc won't return an error?

     

    Thanks,

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor
    One problem I'm having is that the drc returns overlap errors everywhere I use rectangles.  I also have the problem of connecting signals of different names (sub grounds) to one point - it returns overlap errors.  Is there any way to give a rectangle a name or otherwise make it a part of a network so the drc won't return an error?

     

     

    Hi Mike,

     

    RECTs can't be connected to signals. They are non-electical objects. You could use POLYGONs instead. If you want to connect two different signals (with different names) you have to overlap two wires or two polygons....

    This will always bring up a DRC error message.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor
    One problem I'm having is that the drc returns overlap errors everywhere I use rectangles.  I also have the problem of connecting signals of different names (sub grounds) to one point - it returns overlap errors.  Is there any way to give a rectangle a name or otherwise make it a part of a network so the drc won't return an error?

     

     

    Hi Mike,

     

    RECTs can't be connected to signals. They are non-electical objects. You could use POLYGONs instead. If you want to connect two different signals (with different names) you have to overlap two wires or two polygons....

    This will always bring up a DRC error message.

     

    Regards,

    Richard