Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51187 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

    Thanks for all the helps so far, you've been great. I have problem with Eagle and I'm stumped to find an answer. Before I send our boards out I prototype them here. Because we can't do certain operations like running the top layer to thru hole capacitors we need to stop the auto router from running the top layer to those locations. We have been using the restrict layer to keep the top tracks from those locations but this is tedious on larger boards. Is there a simple way we can limit track layers to certain packages? Maybe when 6 comes out if not now?

     

    Thanks,

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Richard,

     

    I'm down to the silkscreen and the files must ship Friday.  Suddenly, the silk screen layers have disappeared!!  They (layers 121 and 122) do not show up in the layers list.  What have I done to make them disappear and what must I do to get them back?  I'm only slightly paniced.

     

    I'm doing two board designs and the silk screen layers show up in one but not the other.

     

    Thanks!

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    I'm down to the silkscreen and the files must ship Friday.  Suddenly,  the silk screen layers have disappeared!!  They (layers 121 and 122) do  not show up in the layers list.  What have I done to make them  disappear and what must I do to get them back?  I'm only slightly  paniced.

     

    I'm doing two board designs and the silk screen layers show up in one but not the other.

     

    Hi Mike,

     

    please try  SET USED_LAYERS ALL;  in the command line.  Does it help?

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    I'm down to the silkscreen and the files must ship Friday.  Suddenly,  the silk screen layers have disappeared!!  They (layers 121 and 122) do  not show up in the layers list.  What have I done to make them  disappear and what must I do to get them back?  I'm only slightly  paniced.

     

    I'm doing two board designs and the silk screen layers show up in one but not the other.

     

    Hi Mike,

     

    please try  SET USED_LAYERS ALL;  in the command line.  Does it help?

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jason,

     

    I see what it is doing now.  When the stop mask layers are on, it throws a DRC error to anything that violates the stop mask - names, values, place, origins.  Whatever is displayed in the image is tested against the stop mask.  So see if there are any real stop mask violations, I'll have to turn off all the layers that print or draw anything other than top and bottom traces and vias and pads etc.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to igalloway

    You're right there. I was just giving an explanation as to why they'd appeared, and if you wanted it to be back as it was before, then how you'd go about it.

     

    I remember the first time I enabled the Stop layers, and was astounded how many DRC errors there were.

     

    Luckily (?) I make my own PCBs, so I don't have a silk screen to worry about image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • igalloway
    igalloway over 14 years ago in reply to e14 Contributor

    Although technically you should respect the DRC errors....and move the

    silkscreen where you can.

    The whole philosophy of DRC is to let the software do the work of finding

    problems.

    At times of course it's too much work to adjust or make corrections (like

    when a silkscreen in a part crosses over some other element, but the use of

    keepouts and restricts are supposed to make your job better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Do the names cross pads (SMT and PTH)? If so, then a DRC error will occur. There's another pair of layers which have been enabled which causes these DRC errors - I can't remember which layers they are though.

     

    Although a quick manual test on an examle board suggests it's _tStop and _bStop. Hide those layers, and the DRCs for them should disappear.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Richard,

     

    Yes, that got the silk layers back and they seem to work ok.  However, there is still weirdness.  DRC returns 1250 errors, all Stop Mask violations caused by the Names.  If I turn the tNames layer off, all those errors go away.  So it is treating the text in the tNames layer as though they are traces.  My other board project does not do this.  Is there some attribute of the Names layer that got changed, maybe?

     

    Thanks,

     

    Michael Watts