Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51140 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi,

     

    I am trying to make a carrier board for a SOM with multiple connectors. Specifically a SOM OMAP-L138: http://www.logicpd.com/products/system-on-modules/omap-l138-som-m1/

     

    The  SOM is using 3 hirose connectors to connect to the carrier board. As the connectors need to be placed very precisely, they recommend machine placement.

     

    How  do you create an eagle device with three connectors that also generates  the neccessary pick-and-place information? I have made a device  already, but it has only one package which includes all 3 connectors, and pick-and-place information is generated per-package.

     

    Do  I really need to make 3 separate devices for the 3 connectors and then  manually place them during board layout? That is a bit of a pain when  having to move the device around.

     

    Nikolaj

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi,

     

    I am trying to make a carrier board for a SOM with multiple connectors. Specifically a SOM OMAP-L138: http://www.logicpd.com/products/system-on-modules/omap-l138-som-m1/

     

    The  SOM is using 3 hirose connectors to connect to the carrier board. As the connectors need to be placed very precisely, they recommend machine placement.

     

    How  do you create an eagle device with three connectors that also generates  the neccessary pick-and-place information? I have made a device  already, but it has only one package which includes all 3 connectors, and pick-and-place information is generated per-package.

     

    Do  I really need to make 3 separate devices for the 3 connectors and then  manually place them during board layout? That is a bit of a pain when  having to move the device around.

     

    Nikolaj

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor
    Do  I really need to make 3 separate devices for the 3 connectors and  then  manually place them during board layout? That is a bit of a pain  when  having to move the device around.

     

    Hi Nikolaj,

     

    yes you have to place the three  connectors separately. I supose you need the exact position of the connectors, so you can use coordinates for exact placement.

    This can look like this: After creating the board you have to MOVE the connectors to their positions

     

    MOVE CON1 (23.3 22.4)

     

    Afterwards you can lock it:  LOCK CON1

     

    If this is a process which has to be done for several layouts you could write a script:

     

    MOVE CON1 (23.3 22.4);

    LOCK CON1;

    MOVE CON2 (25.3 22.4);

    LOCK CON2;

    MOVE CON3 (29.3 22.4);

    LOCK CON3;

     

    Regards,

    Richard