Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
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
  • Replies 1129 replies
  • Subscribers 238 subscribers
  • Views 45985 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel

Top Replies

  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Alessio, I am sorry there is no possibility to allow smaller sizes for a netclasse. The Autorouter has to use the given width. You could pre-route a short piece of the signal manually with the smaller…
  • Richard_H
    Richard_H over 15 years ago in reply to lwathelet +1
    Hi Luc, currently there is no other possibility, sorry. Regards, Richard
  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Edith, the ground layer is an inner layer I suppose. It is defined as a supply layer which is displayed and printed inverted. This means you are not allowed to combine a supply layer with Pads and Vias…
Parents
  • Former Member
    Former Member over 16 years ago

    Hi Richard

    ttanck for yours advices.I m lookinf for a customer a product like this.

    Can you propose me à product CADSOFT (even if near the same)

    thanck

    Fabricant:
    NUMBER ONE SYSTEMS
    Code commande:
    4894121           FARNELL
    Référence fabricant:
    EASY-SPICE

    Conformité RoHS :

    Description
    • SOFTWARE, EASY-SPICE, A/D SIMULATOR
    • Conditions:Windows 95 to XP, Easy-PC for Windows
    • Taille mémoire:64MB
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to Former Member

    Hi again,

     

    I just realized that i did not answer your question about simulating......  sorry.

    EAGLE has no tools to simulate a schematic or parts of it itself. But there is an interface, realized with the help of the User Language, that allows converting data from EAGLE into a simulating software named B2Spice. It's a product of BeigeBag Software in Canada. They realized the ULP for data exchange some years ago. Take a look at their tool at http://www.beigebag.com/eagle.htm

     

    Best regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 16 years ago in reply to Richard_H

    Richard,

    Is Eagle Light capable of importing electronic components from a supplier such as Digi-Key including the Netlist? If so is there a "how to" document I could review?

     

    Thank you.

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to Former Member

    Currently I don't know a tool that allows to import components from, for example, Digikey directly. This would be a task for a EAGLE User Language Program. Provided you have a good data format description of the source files, you could write an ULP that converts this into an EAGLE Library file. For example, look at make-symbol-device-package-bsdl.ulp. It allows to extract all data needed from so-called Boundary Scan Description Language files that are available for lots of complex components.


    You could also have a look at ADI's Ultra Librarian. As far as I am informed you can generate library data for EAGLE, as well.


    There are alos other ULP's that can help in generating library files:

    make-connector.ulp, make_bga.ulp, make_symbol_ulp which are available at www.cadsoft.de/download.htm, ULP directory.

     

    BR,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago in reply to Former Member

    Currently I don't know a tool that allows to import components from, for example, Digikey directly. This would be a task for a EAGLE User Language Program. Provided you have a good data format description of the source files, you could write an ULP that converts this into an EAGLE Library file. For example, look at make-symbol-device-package-bsdl.ulp. It allows to extract all data needed from so-called Boundary Scan Description Language files that are available for lots of complex components.


    You could also have a look at ADI's Ultra Librarian. As far as I am informed you can generate library data for EAGLE, as well.


    There are alos other ULP's that can help in generating library files:

    make-connector.ulp, make_bga.ulp, make_symbol_ulp which are available at www.cadsoft.de/download.htm, ULP directory.

     

    BR,

    Richard