Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 50968 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • VMontoya
    VMontoya over 16 years ago

    Hello Richard,

     

    I am currently with a customer who would like to see some key changes with Eagle:  here is what we discussed:

     

    1 - copy/paste function

    At the moment, he can only copy one schematic.  The scripts don't enable our customer to achieve what he really wants.

    He would like to copy the schematic, the components position on the board and the signal routing.

    This customer works a lot with sub assemblies; if he wishes to copy 20 times the same sub assembly, he has to replace all the components every time on the board.

    Could the enhanced copy/paste facility he is looking for be included in Eagle? 

     

    2 - shortcuts

    He also made a comment about the scripts:  he woud love to have more shortcuts.

    For example, when he is trying to find a component, he would prefer to use CTRL F, rather than have to use scripts.

    The ideal would be to have shortcuts that you can customise.

     

    3 - facilitating the viewing of different layers

    At the moment, our customer has to select a number of Eagle layers (1, 17, 18, 19, 20, 21, 23, 25, 48 et 51) to display the top layers for example.

    What would be great would be if you could assign a key, eg F1, to do this in one go.

    This would make it easier to switch from layers to layers.


    4 - export 3D

    Could you please update the 'generate 3D data' script to enable exporting in the IDF4 format?

     

    5 - packages to be available separately

    The ideal would be to separate the packages from the library.

    This would make it easier for him to create new components, and to switch package from component to component.


    6 - sharing libraries between colleagues

    Could it be possible to access libraries that colleagues create, without having to copy them manually?

     

    Can you please let me know what you think about the above?

     

    Thank you for your help,

     

    Véronique

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to VMontoya

    Hello Véronique,

     

    1 - copy/paste function

     

    The current situation is as follows:

    One can use  the commands GROUP, CUT, and PASTE.

     

    Assumed you have consistent pair of schematic and board and you would like to use one of your existing designs (also a consistent pair
    of sch and brd) in the current project you could begin, for example, with the schematic:
    * Open the schematic you want to use in your project and use the commands GROUP and CUT to copy it into the clipboard
    * Now open the schematic of your current project. You will notice  that the layout editor opens the consistent layout file, too.
      BUT YOU HAVE TO CLOSE IT AGAIN!

    * Now use the PASTE command in the schematic and place the  previously selected group.

    That's it for the schematic.

     

    Now the same procedure for the layout:
    * Open the board you want to put into the clipboard and use   DISPLAY ALL first to activate all layers.
    * Now: GROUP, CUT.

    * Open the "target" layout and PASTE.

     

    Now you have to run the ERC which compares schematic and layout. This is necessary because it might happen that the names of parts or
    nets are renamed while pasting them into the existing project. ERC can check whether the new numbering in SCH and BRD is all the same. In the case there are differences ERC reports this and you have to adjust this manually. Until ERC reports consistency again.

     

    As an alternative there are ULPs that might help. Please take a look at duplicating_vxx.zip or array_board_vxx.zip in the download area of www.cadsoft.de.

     

     

    2 - shortcuts

     

    As Jason already wrote nearly everything can be assigned with a function key. Please see HELP ASSIGN in EAGLE.

     

     

    3 - facilitating the viewing of different layers

     

    EAGLE 5 offers so-called aliases for the DISPLAY command. Select the layers you want to have displayed, do a right mouse click onto the DISPLAY icon, select New from the context menu and name the current display setting. So you can choose it each time you need it with two mouse clicks: Right mouse click onto DISPLAY icon, left mouse click to select it from the context menu.

    More efficient than using a function key, I think.

     

     

    4 - export 3D

     

    The generate-3D project was initiated by one of our EAGLE customers. The author of the ULP would be your contact person. I will forward your request to our development people. I can imagine that this might be something to be implemented in a future EAGLE version.

     

    5 - packages to be available separately

     

    The library structure has grown in the last 20 years. So it's nearly impossible to change it easily. But EAGLE has means to keep the package definitions in the different libraries up-to-date. So take for example look into our ref-packages.lbr. It contains all packages that are used in all the other LBRs (except connectors). If you want to make a change in one of the packages, change it there and UPDATE it in all other LBRs that contain this package. There is an ULP that helps here: run-loop-all-lbr-script.ulp.

     

    6 - sharing libraries between colleagues

     

    Sharing libraries in a network, for example, shouldn't be a problem. But the network administrator has to take care on access rights. If the directory where the libraries are, is read-only, everybody can use, but not change them. If somebody wants to change a library he has to do this with a copy of the lbr file. There should be one person in the team that has to take care on such things and make changes available for all then.

     

     

    Hope this helps.

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hello Richard,

     

    About the copy/paste function requested by Veronique (2010-04-06), did the team work on a true solution ? How can I merge 2 projects (each has more than one sheet and both are already routed) ? Thank you.

     

    Jerome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Alessio,

     

    I am sorry there is no possibility to allow smaller sizes for a netclasse. The Autorouter has to use the given width.

    You could pre-route a short piece of the signal manually with the smaller width and let the autorouter do the rest with 40 mil then.

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

    I hope that this is the right section to submit my question ...
    The question is very straightforward.
    I have a board with power lines that I would do size 40 mil (with net class), but they end not only in big pads but also in pads that have dimensions of 7 mil and so the autorouter fail to connect them and when it is finished connect these by hand is impossible.
    Is there a way to select a preferred width of the track but a tolerance that makes it possible to the autorouter to go down in size where the connection is not possible with the preferred size?
    Thanks
    Alessio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Jerome,

     

    there is no fixed date for version 6, yet. Let's talk about this end of next year again. I am pretty sure that there will be a bit more of information about the planned release date.

    Concerning the ULP: I am sorry, but I believe you are right. It is only for duplicating within one project.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    Thank you for this information. Do you know when the next version that will include this option will be released ?

    I already know the ulp duplicating, but can it be used to duplicate SCH and BRD into another existing project ? I thought it cannot...

     

    Thank you,

    Jerome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Jerome,

     

    there is a new option in the current beta version 5.10.2 that allows to confirm such messages automatically. You can decide for example SET CONFIRM YES; So all the nets will be connected automatically. Maybe this is an option?

    A second idea: There is an ULP available in the CadSoft Download area which promises to duplicate SCH and BRD without loosing consistency. It's named duplicatingxxx. Where xxx stands for a version number I currently do not recall.

     

    Hope this helps.

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    Thank you for your clear answer. About merging 2 or more projects, I have half a solution :

    - On each project, I rename the devices with numbers with offset (I modified the ulp renumber-sheet to do this), for example, in the first projet the devices will be MCU1001, R1001, R1002... in the second project the devices will be MCU2001, R2001...

    - I copy all the boards into the same board.

    - I copy all the sheets into the same schematics.

     

    The problem is now the consistency of the nets, and I didn't find any ulp to rename the nets the same way I do with the devices, and the ulp renamnet-suffix shows a popup for each net... Making an ulp that renames the nets would permit to merge 2 projects in the current EAGLE 5.xx version. Do you have an idea on how to do it ?

     

    In the next version of EAGLE, it would be nice if the sheets of one project could be spread into "folders" or "Tabs".

     

    Thank you,

    Jerome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    Thank you for your clear answer. About merging 2 or more projects, I have half a solution :

    - On each project, I rename the devices with numbers with offset (I modified the ulp renumber-sheet to do this), for example, in the first projet the devices will be MCU1001, R1001, R1002... in the second project the devices will be MCU2001, R2001...

    - I copy all the boards into the same board.

    - I copy all the sheets into the same schematics.

     

    The problem is now the consistency of the nets, and I didn't find any ulp to rename the nets the same way I do with the devices, and the ulp renamnet-suffix shows a popup for each net... Making an ulp that renames the nets would permit to merge 2 projects in the current EAGLE 5.xx version. Do you have an idea on how to do it ?

     

    In the next version of EAGLE, it would be nice if the sheets of one project could be spread into "folders" or "Tabs".

     

    Thank you,

    Jerome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Alessio,

     

    I am sorry there is no possibility to allow smaller sizes for a netclasse. The Autorouter has to use the given width.

    You could pre-route a short piece of the signal manually with the smaller width and let the autorouter do the rest with 40 mil then.

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

    I hope that this is the right section to submit my question ...
    The question is very straightforward.
    I have a board with power lines that I would do size 40 mil (with net class), but they end not only in big pads but also in pads that have dimensions of 7 mil and so the autorouter fail to connect them and when it is finished connect these by hand is impossible.
    Is there a way to select a preferred width of the track but a tolerance that makes it possible to the autorouter to go down in size where the connection is not possible with the preferred size?
    Thanks
    Alessio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Jerome,

     

    there is no fixed date for version 6, yet. Let's talk about this end of next year again. I am pretty sure that there will be a bit more of information about the planned release date.

    Concerning the ULP: I am sorry, but I believe you are right. It is only for duplicating within one project.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    Thank you for this information. Do you know when the next version that will include this option will be released ?

    I already know the ulp duplicating, but can it be used to duplicate SCH and BRD into another existing project ? I thought it cannot...

     

    Thank you,

    Jerome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Jerome,

     

    there is a new option in the current beta version 5.10.2 that allows to confirm such messages automatically. You can decide for example SET CONFIRM YES; So all the nets will be connected automatically. Maybe this is an option?

    A second idea: There is an ULP available in the CadSoft Download area which promises to duplicate SCH and BRD without loosing consistency. It's named duplicatingxxx. Where xxx stands for a version number I currently do not recall.

     

    Hope this helps.

    Richard