Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
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
  • Replies 1129 replies
  • Subscribers 237 subscribers
  • Views 44129 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel

Top Replies

  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Alessio, I am sorry there is no possibility to allow smaller sizes for a netclasse. The Autorouter has to use the given width. You could pre-route a short piece of the signal manually with the smaller…
  • Richard_H
    Richard_H over 15 years ago in reply to lwathelet +1
    Hi Luc, currently there is no other possibility, sorry. Regards, Richard
  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Edith, the ground layer is an inner layer I suppose. It is defined as a supply layer which is displayed and printed inverted. This means you are not allowed to combine a supply layer with Pads and Vias…
Parents
  • Former Member
    Former Member over 15 years ago

    Hi Richard

    I would like to know if it's possible to test Eagle?

    It is possible to simulate the shematic with eagle or an other product(before to do the PCB)

    thanck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to Former Member

    Hi,

     

    there is the EAGLE Freeware you are allowed to use for testing and non-profit use as well. The Freeware has a limitation in the maximum board size of half an Euro card, which is 100 mm x 80 mm, and it is limited to two signal layers (Top and Bottom, no inner layers).

     

    Download is for free from www.cadsoft.de/download.htm or take the link from here at element-14:

    http://www.element-14.com/community/docs/DOC-13200

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago in reply to Former Member

    Hi,

     

    there is the EAGLE Freeware you are allowed to use for testing and non-profit use as well. The Freeware has a limitation in the maximum board size of half an Euro card, which is 100 mm x 80 mm, and it is limited to two signal layers (Top and Bottom, no inner layers).

     

    Download is for free from www.cadsoft.de/download.htm or take the link from here at element-14:

    http://www.element-14.com/community/docs/DOC-13200

     

    Regards,

    Richard