Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51116 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • KennyMillar
    KennyMillar over 16 years ago

    Richard,

     

    Recently we discussed how the keyboard shortcut to flick between schematic and board was disabled in the Mac OS X version of Eagle.

    While I was working today it occurred to me that I can use Mac OS X's 'Spaces' feature - with the board in one space and the schematic in another and this worked great - AND it gives you a really cool sliding animation when you switch between schematic and board.

     

    If you've never used spaces on Mac OS X before I strongly urge you to try it out - it's one of those 'how did we ever manager without this' features.

     

    One minor point though. When I closed the project and openend it again, the windows remembered their size and position on screen, but not which 'space' they were in, so every time I opened the project I had to move the windows to their respective space again.

     

    -Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to KennyMillar

    Hi Kenny,

     

    just tried it and you are right, it's great. As you wrote, once known you don't want to miss it. Thanks for posting and sharing your experience. image

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago in reply to KennyMillar

    Hi Kenny,

     

    just tried it and you are right, it's great. As you wrote, once known you don't want to miss it. Thanks for posting and sharing your experience. image

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Craig,

     

    this is a known problem which is fixed in EAGLE 6.1.0. Please download it from our web site

    http://www.cadsoft.de/downloads/

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    I made a library part with a hole in it.

    After I place this part into my schematic,

    the auto-router is routing traces right through the hole?

    I see the hole is in the DIMENSION LAYER?

    Any idea why the autorouter is doing this?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to igalloway

    Iain Galloway wrote:

     

    Richard,

    I have a couple of items that you could perhaps point me in the right direction.

     

    We have a board design with a large array of the same components...say 1600 diodes.

     

    1) Need to place these on a BRD grid of x by y spaced at nnn apart. I assume this could be done with a ULP or SCR, but I've never really looked into the programming language. Any good starting point for this specifically?

     

    2) Unfortunately when the schematic was first made, a generic diode was just picked, and used a standard part, say 1n4442.

    Now we'd like to replace them ALL with something more custom and have it in our own library where several different footprints can be tried.

    Any ideas here?

    I found a ULP that made a library for the board, but it doesn't actually make the parts on the sch/brd point to that new libraray.

     

     

     

    Hi Iain,

     

    There is an ULP that might help in placing matrix of components or at least giving an example for this. See the cadsoft.de download area, ULP folder. There is  matrizdeleds.ulp

     

    About the diodes: You can use the REPLACE command for this. It could be executed via a script for all diodes in the project. Syntax is:   REPLACE new_device_name component_name;

    Example:

     

    REPLACE 1N4442   D12;

    REPLACE 1N4442   D13;

    REPLACE 1N4442   D15;

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • igalloway
    igalloway over 14 years ago in reply to Richard_H

    Richard,

    I have a couple of items that you could perhaps point me in the right direction.

     

    We have a board design with a large array of the same components...say 1600 diodes.

     

    1) Need to place these on a BRD grid of x by y spaced at nnn apart. I assume this could be done with a ULP or SCR, but I've never really looked into the programming language. Any good starting point for this specifically?

     

    2) Unfortunately when the schematic was first made, a generic diode was just picked, and used a standard part, say 1n4442.

    Now we'd like to replace them ALL with something more custom and have it in our own library where several different footprints can be tried.

    Any ideas here?

    I found a ULP that made a library for the board, but it doesn't actually make the parts on the sch/brd point to that new libraray.