Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51492 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Richard

    I have just made a new library. I can see the library when I open the control panel and brouse in the library directory, its OK

    But when I tray to see / find the new library from windows, I cant see it, but I can see all other library.

     

    When I open my lyberary in Eagle, there is a padlock on all icon

     

    Kind Regards Kenneth K

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Kenneth,

     

    It sounds like your running a windows 7 machine. What you're experiencing is a byproduct of Windows 7's new security features.  The way we get around this is by running EAGLE in compatibility mode.

     

    See the attached text file.

     

    hth,

    Jorge Garcia

    Attachments:
    Get Windows7 to allow modifications to libraries.txt.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Jorge_Garcia

    Okay I'm working on a sort of cartridge:

     

     

    http://www.effector13.com/wp-content/uploads/2011/01/ConsoleCartDevelopmentInfo.jpg

     

     

    I get given some code for this, but I have a problem because it doesn't show up the signal connections OUT,GND, IN...etc. How can you I add those each pad? Do I have to make a new library part? I also need it to be linked back to the schematic too.

     

     

     

     

     

     

     

     

     

    Here's the code if needed:

     

    GRID INCH;

    CHANGE LAYER 20;

    SET WIRE_BEND 2; WIRE 0 (0 0) (1.875 0) (1.875 0.400) (1.975 0.400) (1.975 1.5625)

    (1.8125 1.725) (0.075 1.725) (-0.100 1.5625) (-0.100 0.400) (0 0.400) (0 0);

    CHANGE LAYER 21;

    WIRE 0 (0 0.5) (1.875 0.5) (1.875 0.900) (0 0.900) (0 0.5);

    WIRE 0 (0 0.900) (0 1.500) (0.125 1.625) (1.750 1.625) (1.875 1.5) (1.875 0.9);

    CHANGE LAYER 22;

    WIRE 0 (0 0.5) (1.875 0.5) (1.875 0.900) (0 0.900) (0 0.5);

    CHANGE LAYER 1;

    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)

    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)

    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)

    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);

    CHANGE LAYER 16;

    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)

    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)

    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)

    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);

    CHANGE LAYER 29;

    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)

    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)

    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)

    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);

    CHANGE LAYER 30;

    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)

    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)

    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)

    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);

    VIA 0.029 SQUARE 1-16 (0.0875 0.32) (0.1875 0.32) (0.2875 0.32) (0.3875 0.32) (0.4875 0.32)

    (0.5875 0.32) (0.6875 0.32) (0.7875 0.32) (0.8875 0.32) (0.9875 0.32) (1.0875 0.32) (1.1875 0.32) (1.2875 0.32) (1.3875 0.32) (1.4875 0.32) (1.5875 0.32) (1.6875 0.32) (1.7875 0.32);

     

    Thanks heaps

    GRID INCH;
    CHANGE LAYER 20;
    SET WIRE_BEND 2; WIRE 0 (0 0) (1.875 0) (1.875 0.400) (1.975 0.400) (1.975 1.5625)
    (1.8125 1.725) (0.075 1.725) (-0.100 1.5625) (-0.100 0.400) (0 0.400) (0 0);
    CHANGE LAYER 21;
    WIRE 0 (0 0.5) (1.875 0.5) (1.875 0.900) (0 0.900) (0 0.5);
    WIRE 0 (0 0.900) (0 1.500) (0.125 1.625) (1.750 1.625) (1.875 1.5) (1.875 0.9);
    CHANGE LAYER 22;
    WIRE 0 (0 0.5) (1.875 0.5) (1.875 0.900) (0 0.900) (0 0.5);
    CHANGE LAYER 1;
    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)
    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)
    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)
    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);
    CHANGE LAYER 16;
    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)
    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)
    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)
    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);
    CHANGE LAYER 29;
    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)
    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)
    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)
    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);
    CHANGE LAYER 30;
    RECT (0.0625 0.02) (0.1125 0.32) (0.1625 0.02) (0.2125 0.32) (0.2625 0.02) (0.3125 0.32)
    (0.3625 0.02) (0.4125 0.32) (0.4625 0.02) (0.5125 0.32) (0.5625 0.02) (0.6125 0.32) (0.6625 0.02) (0.7125 0.32) (0.7625 0.02) (0.8125 0.32) (0.8625 0.02) (0.9125 0.32) (0.9625 0.02)
    (1.0125 0.32) (1.0625 0.02) (1.1125 0.32) (1.1625 0.02) (1.2125 0.32) (1.2625 0.02) (1.3125 0.32) (1.3625 0.02) (1.4125 0.32) (1.4625 0.02) (1.5125 0.32) (1.5625 0.02) (1.6125 0.32)
    (1.6625 0.02) (1.7125 0.32) (1.7625 0.02) (1.8125 0.32);
    VIA 0.029 SQUARE 1-16 (0.0875 0.32) (0.1875 0.32) (0.2875 0.32) (0.3875 0.32) (0.4875 0.32)
    (0.5875 0.32) (0.6875 0.32) (0.7875 0.32) (0.8875 0.32) (0.9875 0.32) (1.0875 0.32) (1.1875 0.32) (1.2875 0.32) (1.3875 0.32) (1.4875 0.32) (1.5875 0.32) (1.6875 0.32) (1.7875 0.32);
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi,

     

    the script you are using for creating the cartridge is written for the layout editor. It places VIAs for the connections and it uses rectangles for the SMDs. And that is the problem. A rectangle can't be connected to a signal. It's a simple copper area.......

     

    You have to modify the script and use it in the library in the Package editor. Therefore you have to replace the VIA command with PAD. And you have to replace the rectangles in Top layer with SMDs.

    You can't use the RECT sequence for Top layer because a SMD is placed at it's origin (the center of the SMD).

    Maybe it is easier to run the script in the package editor and replace the rectangles with SMDs afterwards manually.

    For connecting it to the schematic you have to draw a symbol as well.

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi,

     

    the script you are using for creating the cartridge is written for the layout editor. It places VIAs for the connections and it uses rectangles for the SMDs. And that is the problem. A rectangle can't be connected to a signal. It's a simple copper area.......

     

    You have to modify the script and use it in the library in the Package editor. Therefore you have to replace the VIA command with PAD. And you have to replace the rectangles in Top layer with SMDs.

    You can't use the RECT sequence for Top layer because a SMD is placed at it's origin (the center of the SMD).

    Maybe it is easier to run the script in the package editor and replace the rectangles with SMDs afterwards manually.

    For connecting it to the schematic you have to draw a symbol as well.

     

    Regards,

    Richard