Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
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
  • Replies 1129 replies
  • Subscribers 238 subscribers
  • Views 45951 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel

Top Replies

  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Alessio, I am sorry there is no possibility to allow smaller sizes for a netclasse. The Autorouter has to use the given width. You could pre-route a short piece of the signal manually with the smaller…
  • Richard_H
    Richard_H over 15 years ago in reply to lwathelet +1
    Hi Luc, currently there is no other possibility, sorry. Regards, Richard
  • Richard_H
    Richard_H over 15 years ago in reply to Former Member +1
    Hi Edith, the ground layer is an inner layer I suppose. It is defined as a supply layer which is displayed and printed inverted. This means you are not allowed to combine a supply layer with Pads and Vias…
Parents
  • VMontoya
    VMontoya over 15 years ago

    Hello Richard,

     

    I am currently with a customer who would like to see some key changes with Eagle:  here is what we discussed:

     

    1 - copy/paste function

    At the moment, he can only copy one schematic.  The scripts don't enable our customer to achieve what he really wants.

    He would like to copy the schematic, the components position on the board and the signal routing.

    This customer works a lot with sub assemblies; if he wishes to copy 20 times the same sub assembly, he has to replace all the components every time on the board.

    Could the enhanced copy/paste facility he is looking for be included in Eagle? 

     

    2 - shortcuts

    He also made a comment about the scripts:  he woud love to have more shortcuts.

    For example, when he is trying to find a component, he would prefer to use CTRL F, rather than have to use scripts.

    The ideal would be to have shortcuts that you can customise.

     

    3 - facilitating the viewing of different layers

    At the moment, our customer has to select a number of Eagle layers (1, 17, 18, 19, 20, 21, 23, 25, 48 et 51) to display the top layers for example.

    What would be great would be if you could assign a key, eg F1, to do this in one go.

    This would make it easier to switch from layers to layers.


    4 - export 3D

    Could you please update the 'generate 3D data' script to enable exporting in the IDF4 format?

     

    5 - packages to be available separately

    The ideal would be to separate the packages from the library.

    This would make it easier for him to create new components, and to switch package from component to component.


    6 - sharing libraries between colleagues

    Could it be possible to access libraries that colleagues create, without having to copy them manually?

     

    Can you please let me know what you think about the above?

     

    Thank you for your help,

     

    Véronique

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to VMontoya

    Hello Véronique,

     

    1 - copy/paste function

     

    The current situation is as follows:

    One can use  the commands GROUP, CUT, and PASTE.

     

    Assumed you have consistent pair of schematic and board and you would like to use one of your existing designs (also a consistent pair
    of sch and brd) in the current project you could begin, for example, with the schematic:
    * Open the schematic you want to use in your project and use the commands GROUP and CUT to copy it into the clipboard
    * Now open the schematic of your current project. You will notice  that the layout editor opens the consistent layout file, too.
      BUT YOU HAVE TO CLOSE IT AGAIN!

    * Now use the PASTE command in the schematic and place the  previously selected group.

    That's it for the schematic.

     

    Now the same procedure for the layout:
    * Open the board you want to put into the clipboard and use   DISPLAY ALL first to activate all layers.
    * Now: GROUP, CUT.

    * Open the "target" layout and PASTE.

     

    Now you have to run the ERC which compares schematic and layout. This is necessary because it might happen that the names of parts or
    nets are renamed while pasting them into the existing project. ERC can check whether the new numbering in SCH and BRD is all the same. In the case there are differences ERC reports this and you have to adjust this manually. Until ERC reports consistency again.

     

    As an alternative there are ULPs that might help. Please take a look at duplicating_vxx.zip or array_board_vxx.zip in the download area of www.cadsoft.de.

     

     

    2 - shortcuts

     

    As Jason already wrote nearly everything can be assigned with a function key. Please see HELP ASSIGN in EAGLE.

     

     

    3 - facilitating the viewing of different layers

     

    EAGLE 5 offers so-called aliases for the DISPLAY command. Select the layers you want to have displayed, do a right mouse click onto the DISPLAY icon, select New from the context menu and name the current display setting. So you can choose it each time you need it with two mouse clicks: Right mouse click onto DISPLAY icon, left mouse click to select it from the context menu.

    More efficient than using a function key, I think.

     

     

    4 - export 3D

     

    The generate-3D project was initiated by one of our EAGLE customers. The author of the ULP would be your contact person. I will forward your request to our development people. I can imagine that this might be something to be implemented in a future EAGLE version.

     

    5 - packages to be available separately

     

    The library structure has grown in the last 20 years. So it's nearly impossible to change it easily. But EAGLE has means to keep the package definitions in the different libraries up-to-date. So take for example look into our ref-packages.lbr. It contains all packages that are used in all the other LBRs (except connectors). If you want to make a change in one of the packages, change it there and UPDATE it in all other LBRs that contain this package. There is an ULP that helps here: run-loop-all-lbr-script.ulp.

     

    6 - sharing libraries between colleagues

     

    Sharing libraries in a network, for example, shouldn't be a problem. But the network administrator has to take care on access rights. If the directory where the libraries are, is read-only, everybody can use, but not change them. If somebody wants to change a library he has to do this with a copy of the lbr file. There should be one person in the team that has to take care on such things and make changes available for all then.

     

     

    Hope this helps.

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Richard_H

    As a sort of follow-on from your reply to Véronique, I really do like the right-click to get the list of the most recently used components - however, is there a way to increase the number in the list?

     

    I might have missed it in the documentation...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to Richard_H

    As a sort of follow-on from your reply to Véronique, I really do like the right-click to get the list of the most recently used components - however, is there a way to increase the number in the list?

     

    I might have missed it in the documentation...