Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51186 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Gary,

     

    as you just did...  image

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    How do I ask Richard questions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hello again,

     

    I am not sure what you exactly want to do....

    As far as I understand you want to write an ULP that places vias in your layout, correct?

    So you have to write an ULP that executes commands in the EAGLE layout editor. It is useful to let the ULP create a script (which contains a number of EAGLE commands executed subsequently) for your purose. Look into one of the ULPs in order to get out how this works, for example into change-via-by-stack.ulp:

     

    Here a short part of it where we create a script file that will be executed:


    board(B) {
        script = filesetext(B.name, ".scr");
        output(script, "wtD") {  // temporary file
          set_layer();
          B.signals(S) {
            S.vias(V) {
              if (V.start == via_start && V.end == via_end) {
                if (stack) printf("CHANGE VIA %s (%.4f %.4f);\n", new_stack, u2mm(V.x), u2mm(V.y) );
                else {
                  if (v_shape) printf("CHANGE SHAPE %s (%.4f %.4f);\n", v_shape, u2mm(V.x), u2mm(V.y) );
                  if (strupr(argv[3]) != "NO") {
                    if (v_drill) printf("CHANGE DRIL %.4f (%.4f %.4f);\n", v_drill, u2mm(V.x), u2mm(V.y) );
                    else         printf("CHANGE DRIL (%.4f %.4f);\n", u2mm(V.x), u2mm(V.y) );
                    if (v_diam)  printf("CHANGE DIAM %.4f (%.4f %.4f);\n", v_diam, u2mm(V.x), u2mm(V.y) );
                    else         printf("CHANGE DIAM (%.4f %.4f);\n", u2mm(V.x), u2mm(V.y) );
                  }
                }
              }
            }
          }
          printf("GRID LAST;\n");
          printf("DISPLAY NONE ");
          B.layers(L) if (L.visible) printf(" %d", L.number);
          printf(";\n");
        }
      }

    dlgDialog("test") {
      string text;
      int t = fileread(text, script);
      dlgTextEdit(text);
      dlgHBoxLayout {
        dlgPushButton("OK") dlgAccept();
        dlgPushButton("esc") { dlgReject(); exit(-1); }
        dlgStretch(1);
      }

    ........................

    ........................

    ........................

     

      exit("SCRIPT '" + script + "'\n");

     

    The output() statement creates the file, printf() writes the commands into the file. exit() executes the script file.

     

    Hopehis helps......

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Dear Richard,

    Again, sorry for my bad english image. I have a task to draw my schools symbol from vias, using ulp. I can calculate the coordinates for the vias in my ulp, but I can't draw any. In my another discussion you answered me, that is have to use a script. My question now is how can I autorun and than delete the script after the ulp was executed?

    Thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi K Sz,

     

    I do not fully understand what you would like to do, but if you want to place a pad... This can be only done in the library in the package editor. In the layout editor you have to use a VIA. Or do you want to place a component in the layout?

    Could you please give me some more information?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,
    I'm using Eagle 5.11 and i have a task to write an ulp, that draws a logo from pads. My question is: why i can't draw a single pad with ulp? This is my only obstacle and i cannot finish my ulp. I would like to know, how to draw pad with ulp. I looked in some files, but unfortunately it didn't help. Sorry for my bad english. image
    Thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joe,

     

    you can use two pads as well. Best would be then to use two pins and connect them both with the signal....

    Currently there is no better solution. We have to wait for EAGLE version 6. There we will have the possibility to connect one pin to several pads and it will be possible to draw arbitrary pad shapes with a POLYGON or WIREs. There won't be DRC errors and polygons in the layout will be connected or isolated properly.

     

    Best regards,

    Richard

     

    BTW: You know that "Adler" is the German word for "eagle"?  SCNR...  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Robert,

     

    you have to draw restricted areas. As far as I know there are some ULPs that could help here. It is possible to route the nets by classes, there is a ULP that draws restricted areas on all pads on top layer. please look at http://www.cadsoft.de/downloads/user-language-programs/ and use the search function. "auto" should give some results.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Richard,

    Thanks for the quick reply.

    I find that when I make the library part, if I just add another square pad to cover one round end of the test point pad, I wind up with the shape I need wiithout having to draw any polygons.

    The stop layer is made automatically and shows up on the PCB when I enable the layer to see it.

    The only problem I still have is that when I connect the PAD to ground and pour a ground plane, the section of the PAD that is made by the square does not connect to ground.  The other part of the pad (the part with the two rounded ends) connects just fine.

    I was thinking of making another PAD that would have a separate connection for both pads and I would just connect both to ground on the schematic.

    I hope this makes sense.  Anyway, thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

    Thanks for all the helps so far, you've been great. I have problem with Eagle and I'm stumped to find an answer. Before I send our boards out I prototype them here. Because we can't do certain operations like running the top layer to thru hole capacitors we need to stop the auto router from running the top layer to those locations. We have been using the restrict layer to keep the top tracks from those locations but this is tedious on larger boards. Is there a simple way we can limit track layers to certain packages? Maybe when 6 comes out if not now?

     

    Thanks,

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>