Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51182 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    I figured there had to be some reasonable way to do it.  That is tooooo easy!

     

    Thanks a ton, Richard!

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Mike,

     

    yes of course there is.... image

    Please arrange the EAGLE Control Panel and the Library Editor window with the target library on the Desktop so that you can see both windows. Now expand the Libraries entry of the tree view in the EAGLE Control Panel and click onto the Device you want to copy into your target lbr. Drag&Drop the entry into the Library Editor
    window.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi K Sz,

     

    why re-inventing the wheel? There are ULPs that generate a BOM with attributes including. Look at:

    http://www.cadsoft.de/cadsoft-downloads/

    bom_with_attributes.zip

    bom-ex.zip

    attbom.zip

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Anna,

     

    there a ULPs that generate a script file that will be executed automatically. Look into my posting some messages above repying to KSz. There is you can see some lines of change-via-by-stack.ulp that might help. By the way: The User Lanugae is completely documented in the EAGLE help. You can also download this part of the help as PDF from http://www.cadsoft.de/downloads/documentation/

    There an ulp5110-en.pdf available.

     

    Hope this helps.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Hi Richard,

     

    Thanks. 

     

     

     

    Gary Weitzman

     

    President

     

    GDW Enterprises

     

    25645 La Cima

     

    Laguna Niguel, Ca 92677

     

    714 504 6639

     

    fax 949 364 1502

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Garry,

     

    yes EAGLE 5.x works with Windows 7 64-bit.

     

    Reagrds,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

     

    I want to copy a device from an existing library and put the copy in a different library.  I would rather not have to go back and forth copying first the symbol, and then the package and then make the new device in the new library.  Isn't there a way to just copy a whole device to a new library?

     

    Thanks!

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Richard,

    Thank you for your help, it was very useful.

    Here is my other task:
    I have to write a ulp, that makes a list of the used parts of a schematic. So if i add a resistor to the schematic, the ulp will make a list with one resistor and the attributes of the resistor (for example: resistor 1: 100Ohm, etc.).
    Thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi there,

     

    I wish to write a simple ulp that generates a script.

     

    I know what I want the script to say (a simple series of name commands), generated using a couple of inputs (a starting index and the desired naming prefix).

     

    I need to run similar scripts for different starting inputs over 70 times to cover all the replicated blocks on my board, so I want to write a ulp to generate the script for me.  I know this should be straightforward, but I'm quite unfamiliar with the syntax etc.

     

    I have the user language manual, which is helpful but a little overwhelming when first starting!  I'm just hoping someone could point me to a simple ulp that takes a couple of inputs and generates a script that I can look at as an example.  I'm getting hopelessly lost looking at some of the bigger ulps which are doing all sorts of fancy things I don't need at this point...

     

    Any assistance appreciated - feel free to point me to previous discussion on this point if there is one that I've failed to find.

     

    Many thanks,

    Anna

     

    EDIT: I have spent the day playing and have finally managed to write a ulp that successfully generates the required scripts. So, no need to respond to this query.

    Thanks for this helpful thread though!  I would like to suggest that a tutorial on ulp-writing would be a helpful addition to the available documentation in future.

    Regards,

    Anna

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Hi Richard,

     

    Does 5.6 work with win7 64 bit?

     

     

     

    Regards,

     

     

     

    Gary Weitzman

     

    President

     

    GDW Enterprises

     

    25645 La Cima

     

    Laguna Niguel, Ca 92677

     

    714 504 6639

     

    fax 949 364 1502

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>