Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51059 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • ian_byrne@bose.com
    ian_byrne@bose.com over 14 years ago

    For the LIFE of me I cannot figure out what to do to import my.dxf file which has a board outline that I need to create a board.

    I am not sure what to do with a .scr file after I convert it......anyone got any steps I can follow?

    Sorry for being a complete novice!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to daomsk

    Hi Alex,

     

    there is documentation available for make-symbol-device-package-bsdl.ulp. It is part of the EAGLE installation and located in the eagle/doc folder and named 

    make-symbol-device-package-bsdl-2011-en.pdf.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Mike,

     

    ROUTE as an icon is exactly the same as typing it in the command line. No difference.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • daomsk
    daomsk over 14 years ago in reply to Richard_H

    Hi Richard,

    Please help to understand the script make-symbol-device-package-bsdl.ulp.

    Unfortunately, there is no description of this script, and I can not figure out how to properly create text or BSDL files.

    On the Internet, could not find examples of the use this script.

    Thanks in advance, Alex



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Richard,

     

    I fiddled with it and got it cleaned up.  Not exactly sure why it was doing what it was doing.  But I deleted the connection on the schematic, ripped up each end segment of the trace, remade the connection on the schematic and re-routed each end segment. 

     

    When you say ROUTE command, are you referring to using the icon from the tool bar on the left?  I presume so, and I guess it is a command.  But it seems more like a tool than a command.  Is there significance to entering a command on the command line?  I did enter ROUTE on the command line and it did nothing of significance other than select the Route tool.  I presume this is all the same, right?

     

    Thanks, it was your suggestion of using Route that got me going on it again.

     

    Thanks,

     

    Michael Watts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to Dusan_R

    Hi Dusan,

     

    I will keep you message in mind and look into the Design Rules subject we discussed here as soon as I have a bit of time for this. Seems to be a bit odd....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Mike,

     

    what about ROUTE? When you try to route it does this help? You could also check with MOVE what the matter is. Maybe there are several wires at this position..... Once you got out what the problem is you can use UNDO to get back the original situation. Then decide how to proceed.

    If you are unsure, send me your board file with private mail to support@cadsoft.de

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Mike: I would check the name of the trace to see if it's the same name as the air wire. I would understand it if it was a different name, and the traces aren't exactly on the start and end pad central position.

     

    Also, does a DRC check show any errors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hey Richard,

     

    I changed a few things on a board and now it gives me an air wire between two IC pins yet there is clearly a trace between them.  The trace is named the same as the connection on the schematic.  I can't seem to get the airwire to go away.  What should I do?  I'm using 5.11.

     

    What I don't want to do is rip up the whole trace and reroute it since it's a complicated trace.

     

    Thanks,

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Yes, I might have done it. But everytime I reopen Eagle, the design rules

    are declared default, even though they are set correctly. Also in the XML

    data there is the header and description of the defaul rules instead of the

    rules I have in used indeed. Only after I load the rules from the file I

    have saved it looks OK - but only before the session is closed. A bit

    confusing...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>