Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Problemme de conexion dans la shematic d'eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 673 views
  • Users 0 members are here
Related

Problemme de conexion dans la shematic d'eagle

e14 Contributor
e14 Contributor over 16 years ago

bonjour

Je n'arrive pas a connecter deux composants. Les composants sont bien sur la grille.

Par moment je peut connecter et par moment je ne peut pas. Il me faut par moment passer plusieurs longues minute pour connecter des composants.

Si quelqu'un à déjà eu ce problème peut il me dire comment le corriger.

Merci d'avance

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Bonjour Cyril,

     

    j'espère que ma réponse est compréhensible en anglais. Mon français est trop mauvais.....

     

    There a few items you have to take care on:

    Be sure to use the default grid of 0.1 inch in the schematic. All parts have to be placed in this grid. All nets have to be drawn in this grid.

     

    Nets have to start and end exactly in a pin connection point. In order to see this point, please display layer 93, Pins. Now will see a green circle at one end of a pin. There the net must start/end.

     

    Use the NET command, not WIRE.

     

    Don't copy nets with the COPY command. The net name of the copied part will be unchanged. So these nets will have the same signal.

     

    Don't use the MOVE command in order to move a net onto a pin connnection point. The net won't be connected with the pin.

     

    If you are moving a component's pin onto another pin (connection point onto connection point), and both pins are not yet connected to a net, they will be connected!

    If one of the pins is already connected with a net, moving one pin over the other won't establish a connection.

     

    Moving a component's unconnected pin onto a net, will establish a connection between net and pin.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago

    Bonjour Cyril,

     

    j'espère que ma réponse est compréhensible en anglais. Mon français est trop mauvais.....

     

    There a few items you have to take care on:

    Be sure to use the default grid of 0.1 inch in the schematic. All parts have to be placed in this grid. All nets have to be drawn in this grid.

     

    Nets have to start and end exactly in a pin connection point. In order to see this point, please display layer 93, Pins. Now will see a green circle at one end of a pin. There the net must start/end.

     

    Use the NET command, not WIRE.

     

    Don't copy nets with the COPY command. The net name of the copied part will be unchanged. So these nets will have the same signal.

     

    Don't use the MOVE command in order to move a net onto a pin connnection point. The net won't be connected with the pin.

     

    If you are moving a component's pin onto another pin (connection point onto connection point), and both pins are not yet connected to a net, they will be connected!

    If one of the pins is already connected with a net, moving one pin over the other won't establish a connection.

     

    Moving a component's unconnected pin onto a net, will establish a connection between net and pin.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Richard_H

    Merci pour cette réponse rapide.

    Mon anglais n'est vraiment pas terrible c'est pourquoi je parle en français mais j'arrive à lire l'anglais, il n'y a pas de problème.

    Mes composants sont placer sur une grid au pas de 0.635mm (soit 1/4 de 0.1inch).

    J'ai utiliser la commande NET mais rien n'y fait cela ne fonctionne toujours pas.

    Sur un CI j'arrive à connecter des pin mais pas toutes. Par moment quand je suprime le NET et le refait cela fonctionne mais c'est aléatoire sur le nombre de fois à éffectuer cette manoeuvre.

    J'ai remarquer aussi que cela ce passait par des périodes. j'ai eu des période ou EAGLE fonctionnait très bien sans aucun soucis et j'ai et des périodes ou EAGLE ne fonctionnais pas très bien (problème de connection dans la schematic).

     

    Cordialement,

     

    Cyril