Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How can I create several boards based on one schematic?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 191 subscribers
  • Views 985 views
  • Users 0 members are here
Related

How can I create several boards based on one schematic?

MX21
MX21 over 16 years ago

I am designing a board that will have 3 variations:

 

   1) full function unit with display, memory, and external interface.

   2) same as 1, but without the memory and interface.

   3) same as 1, but without the display, memory and interface.

 

Is there a way to do 3 board layouts based on the same schematic?

This way, common areas of the design that change will be changed for all variations.

 

Is there a way to mark parts in the schematic as not being installed in some of the board layouts?

For example, the display part footprint only needs to exist on variations 1 and 2.

 

Thanks,

 

MX

  • Sign in to reply
  • Cancel
Parents
  • huayuliang
    huayuliang over 16 years ago

    Don't do that!

     

    they are different variant or branch for your project.

     

    just copy it and give them related name.

     

    if you warry about the synchronous update of three project in EAGLE, you can replace the schematic file from newer.

     

    just a few advice , maybe it is wrong..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to huayuliang
    What I did for a similar product is use one board file, but draw 3 different board in there, first starting at (0,0mm) second at (0,100mm), third at (0,200mm). Works great, board house had no problems with this solution.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • huayuliang
    huayuliang over 16 years ago in reply to e14 Contributor

    yes,  if you want put them together in a unrelated brd file, and send to board house, it is right.

    because this will not affect their source schematic and board file.

     

    There is a ulp on CADSoft download area to work for this, but I only remembered a part of name, "pan....ulp", sorry.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to huayuliang

    There is a ulp on CADSoft download area to work for this, but I only remembered a part of name, "pan....ulp", sorry.

     

    Its name is panelize.ulp and comes with the EAGLE installation.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago in reply to huayuliang

    There is a ulp on CADSoft download area to work for this, but I only remembered a part of name, "pan....ulp", sorry.

     

    Its name is panelize.ulp and comes with the EAGLE installation.

     

    Regards,

    Richard