Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Device TJA 1054 and S912XEQ512
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 425 views
  • Users 0 members are here
Related

Device TJA 1054 and S912XEQ512

e14 Contributor
e14 Contributor over 15 years ago

Hello,


I am a new user  Eagel, i work with free version for test because and i want to buy the pro version.

I do not find some device as TJA 1054 from NXP and S19XEQ512 from freescale, i update the librairy but impossible to find these device.

If i buy the pro version,  is it probable to find these device or the librarys are identical in all version eagle ?

 

I know that if i dont find the compenent, i must create it.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,

    I find a solution for my quetion, the package for S19XEQ512 is 80QBP in the library micromotorola and the package for TJA1054 is the same of TJA 1040 in the library NXP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,

    I find a solution for my quetion, the package for S19XEQ512 is 80QBP in the library micromotorola and the package for TJA1054 is the same of TJA 1040 in the library NXP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi,

     

    just as an addendum:

    EAGLE comes with a library named ref-packages.lbr which contains all the packages which are used in all the other libraries (exeption are connectors).

    For searching a package use the search line of the ADD command in the Layout Editor. If you are looking for devices, use the ADD command in the Schematic Editor.

     

    Regards,

    Richard