Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum create strap
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 752 views
  • Users 0 members are here
Related

create strap

e14 Contributor
e14 Contributor over 14 years ago

hello all i come here for the seconds time because Baby eagles Torture me.

 

I have finish to root my card but i  would be doing 2 last connexions and i need to create a straps  (bridges in top face) .
For that i would like use the fonction "follow-me"  but when i try this option eagles told me "ERROR  IN PARAMETERS CHECK ROUTING GIRD ! "

 

I have check the parameters of routing gird and i have not see where is the probleme ... !

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi again,

     

    IMHO 1mm might be to coarse. Depending on the components you are using you can take a gridf of 0.5mm/0.1mm

    or maybe imperial based 50/25/12.5/6.25/3.125 mil.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Oh thank it''s true it's a probleme  of  gird i have 0.0001 mm and he have no probleme when i use a gird of 1mm  but he have not lot of precision Oh thank it's true it's a problem  come of  grid  i had use "0.0001 mm". I have no problem when i use a grid of 1mm  but i lose the  precision

     

     

    For the moment it's ok thanks !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago

    Hi,

     

    what is the routing grid you are working with? For the follow-me router it is the grid you have set in the layout editor.

     

    Regards,

    Richard