Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Problems panning in Eagle v7.2.0 on Mac
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 352 views
  • Users 0 members are here
  • eagle
  • osx
  • mac
Related

Problems panning in Eagle v7.2.0 on Mac

e14 Contributor
e14 Contributor over 11 years ago

Running CADsoft Eagle (Standard Ed.) v7.2.0 on a Mac OSX 10.9.5

I have trouble panning with the trackpad using 2 fingers....sometimes it works, sometimes it does not.

Anyone had similar problems?

Anyone found a fix?

Thx

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Additional icon and command to view full library structure with one click

    Additional information in the Control Panel available:

    Devices, packages and symbols are now visible in a reorganized structure. The symbols were added and can be previewed

    Package-Description list: the related symbol keeps showing while scrolling through the list

    Direct access to Reference Manuals, accessible without leaving EAGLE

    64bit version of EAGLE is now available

    for improved performance on Windows, Linux and Mac and simplified Linux installation.

    Keeping up with the trend towards 64bit machines, EAGLE now leverages the improved performance of the 64bit architecture.

    Significantly extended IDF export option

    for 3D view and STEP File export

    Update to the latest UI framework from QT

    Had the same problem. Fortunately, it's an easy fix!

    Options > User Interface...

    Set mouse wheel zoom to 0.

    Turn Legacy mouse wheel mode off.