Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum non rectangular pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 893 views
  • Users 0 members are here
  • pad
  • package
  • custom
  • Design
Related

non rectangular pad

jekain314
jekain314 over 10 years ago

The Murata LXDC2HL series part is a micro-sized DC-DC converter with four pads.

One is rectangular with a clipped corner as a orientation marker. I included the land layout from the spec sheet.

Is there an easy way to make this non-standard pad?

Or does anyone have a package design for this part?

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    James,

     

    The solution is to draw a standard pad or pads as rectangles and then use the polygon tool to draw the "non-rectangle" parts of the pad.  Just make sure to use "1 Top" as the layer for the polygon and select polygon pour of "Solid".  The net result is a pad with some extra pour adjacent to the pad to create the shape you need in the foot print.  You can also use multiple Pads in the foot print and by rotating and overlapping them create the pad you show below.  You can then assign them all to the same symbol pin when you create the device in eagle. Connect the pins and pads using the connect button and the you can use the append button to append additional pads to the pin.  You would do this if had drawn several overlapping pads to create a unique pad shape which is an alternative to adding a polygon pour adjacent to the pad.

     

    Hope this helps... Sorry for being lazy and not taking screen shots.

     

    Regards,

    Rob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jekain314
    0 jekain314 over 10 years ago in reply to e14 Contributor

    Thanks for the detailed solution ..

    Jim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jekain314
    0 jekain314 over 10 years ago in reply to e14 Contributor

    Thanks for the detailed solution ..

    Jim