Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Reticon SAD1024 Delay Chip
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 39 replies
  • Answers 14 answers
  • Subscribers 203 subscribers
  • Views 13436 views
  • Users 0 members are here
Related

Reticon SAD1024 Delay Chip

Andy Betts
Andy Betts over 8 years ago

Reaching out to the people on this web site.......

 

I'm after a SAD1024 delay chip, they were manufactured by Reticon and are now discontinued, and have been for around 30 years. I'm hoping someone here may have one lying around....... if so can you get back to me and I'll make you an offer to buy it off you.

 

As a heads up this is required for a planned pedal build, for the near future, but it all rests on being able to obtain this IC chip.

 

The data sheet is available to read here

 

http://www.pmerecords.com/Docs/Archer_SAD-1024_Tech_Data.pdf

  • Sign in to reply
  • Cancel
  • Andy Betts
    0 Andy Betts over 8 years ago

    I've done some digging, and a while ago a company called Hartman brought out a clone of this pedal... I don't believe they sell it any more, but i could try looking for a schematic for that. From all the write ups I've read, it's exactly the same as the old Electric Mistress however I believe they substituted a different IC in that position. Unfortunately I've yet to find a schematic for that pedal as it's a boutique pedal, and these manufacturers are fiercely secretive about releasing schematics for their pedals.

     

    Here's a You Tube video that AB tests the Hartman against a genuine Electric Mistress..... I need to find out what components they used.

     

    He does say in this video that the Hartman uses the same delay chips as the original... Which may be true, and also might answer why they don't make them any more

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago

    This would be a good circuit to duplicate using a Cypress Semiconductor PSOC board with its programmable Analog and digital components.

     

    You could integrate a robust analog section for detection and then use a software controlled counter to establish the precise delay you need.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to Andy Betts

    I thought about making a replica using modern bits, ADC , digital processing, DAC. Because of the way the chip works an exact replica is tricky:

     

    For an approximation:

    AD SSM2604, 24 bit 96kHz sample rate dual ADC/DAC for about £5 from Farnell, controlled by a little FPGA or possibly a DSP - the parts shouldn't cost more than £20 in total but you will need a PCB and the software won't be easy.

     

    To make an exact duplicate is harder because the original chip samples at up to 2MHz and you would need to use SAR ADCs and a fast DAC  - parts up to maybe £60 or even more.

     

    So, for the time being , it's probably better to just bite the bullet and cough up for the old bits.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 8 years ago in reply to michaelkellett

    EBay, they go for anything from £70 to well over £100 each

     

    https://www.ebay.co.uk/sch/i.html?_from=R40&_trksid=m570.l1313&_nkw=sad1024&_sacat=0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to jw0752

    John Wiltrout wrote:

    Hi Andy,

    There was some talk on the following link about using a MN3007 as a possible substitute.

     

     

    The MN3001 looks a better match. It's got two, independent 512-stage delays like the SAD1024.

     

    There are some for sale here

     

    https://www.cricklewoodelectronics.com/MN3001.html

     

    Not pin-for-pin. Might be that it could be made to work in the same circuit (I haven't looked at the datasheets in detail, so don't quote me on that). One obvious difference is that it has an additional Vbb supply which you'd have to generate (a substrate bias to stop it latching up and toasting itself when the clocks overshoot).

     

    Perhaps consider a small adapter board that would plug in and replace a SAD1204.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to Andy Betts

    How much do you have to pay for an original chip ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 8 years ago in reply to michaelkellett

    Hi Michael

     

    Yeah, I know small bear... US supplier, and expensive to get shipped over to the UK.

     

    The circuit is attached

     

    image

     

    From what I understand, the SAD1024 is pretty peculiar to this circuit, however if there's a good substitute I'm willing to look into that.

     

    Original SAD chips are expensive, for that very reason....... They are gold

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to jw0752

    Andy,

    You may know these people:

     

    Small Bear Electronics

     

    They have clones of the MN3207 chip.

     

    Why must you have the SAD1024, can you post the circuit of the thing you want to build. It is possible to make a replacement for the SAD1024 using an ADC, tiny FPGA and DAC - it won't be the same size (on a hobby budget) but would work fine, and offer all sorts of other possibilities.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago

    Hi Andy,

    I checked and I do not have this chip. Apparently it was sold for a while by Radio Shack under stock number 276-1761. There was some talk on the following link about using a MN3007 as a possible substitute.

     

    http://music-electronics-forum.com/t23353/

     

    I see that there are two or three listed on ebay but the sellers know they have little pieces of gold judging by the price tags.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<