Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to easily connect different nets in Layout?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 190 subscribers
  • Views 793 views
  • Users 0 members are here
Related

How to easily connect different nets in Layout?

e14 Contributor
e14 Contributor over 16 years ago

     I'm laying out a multilayer PCB with several dense BGA packages. I've got the schematic all ready and I'm getting into the layout. Under the BGAs the first thing I did is to place a small via next to each BGA pad (for the dog-bone routing approach).

     The problem is that when I connect the nearby pad to the new via, the signals don't connect. The pad may have a name like 'Signal_A', and the new via will have the autogenerated net name like 'N$527'. I know I can manually change the net each via is on so that the routing will actually connect the signals, but that is a very large task considering the many hundreds of BGA pins in the design.

     I seem to remember somehow figuring out how to do this in previous designs (I have used Eagle for a while, but never for a design this complex), but I can't remember what I did. I remember being able to just drag the trace from the properly named pad over to the new via and dropping it, and have the via automatically accept the name of the net. Did I completely imagine this? I'm too young to have this kind of bad memory!

 

Thanks for your help. Eagle is such a great product!

 

Steve

  • Sign in to reply
  • Cancel
  • huayuliang
    0 huayuliang over 16 years ago in reply to e14 Contributor
    yes, these combination of mouse and  key make route very easy, only a few key.. I like this.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Yes, Absolutely.

     

    Also, the following Mouse key combinations might help you for any further routing...

     

    Ctrl+Left starts routing at any given point along a wire or via.
    Shift+Left starts routing with the same width as an existing wire.
    Center selects the layer.
    Right changes the wire bend style

    Shift+Right reverses the direction of switching bend styles.
    Ctrl+Right toggles between corresponding bend styles.
    Shift+Left places a via at the end point.
    Ctrl+Left when placing a wire end point defines arc radius.

     

    Best Regards,

    Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to ira

    Hi Ira,

     

    If you have a 3-button mouse, use the middle click while dragging the route to change from top to bottom and vice versa.

     

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ira
    0 ira over 16 years ago in reply to Richard_H

    Now that I've got the via where I want it, is there an easy way to have the trace change to the next layer? For me I just want the other side as I only do 2 layer boards.

     

    Ira

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Richard_H

    That is a very handy thing to know.

     

    Thanks for the hint!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 16 years ago

    Hi Steve,

     

    easiest way: Use ROUTE, click onto the pad, and move the trace to the position where the via should be placed. Now Shift + left mouse click places the via.

    HTH

     

    Regards,
    Richard