Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum can only display one layer's polygon plane of copper?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 553 views
  • Users 0 members are here
Related

can only display one layer's polygon plane of copper?

huayuliang
huayuliang over 16 years ago

I often need view the only one rastsnested polygon of two layers, but the rastsnested polygon top layer will block my view.

such as I'm place via to connect ground plane between the top layer and bottom layer, and the other case..

 

of cause I can cancel the display of top layer, but I need view the top layer, just don't need process polygon when rastsnest.

 

 

it is too hard for my bad english..sorry.

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 16 years ago

    Hello,

     

    to bring the polygon back into the outlines mode, use RIPUP and click onto the polygon's contour.

     

    There are some options for RATSNEST and RIPUP that might help. I simply take it from the help:

     

     

     

    The RIPUP command changes routed wires (tracks) into airwires. That can be done for:

    • all signals (RIPUP;)
    • all signals except certain ones (e.g. RIPUP ! GND VCC;)
    • one or more signals (e.g. RIPUP D0 D1 D2;)
    • certain segments (chosen with one or more mouse clicks)
    • all polygons (RIPUP @;)
    • all polygons of certain signals (e.g. RIPUP @ GND VCC;)
    • all polygons except those of certain signals (e.g. RIPUP @ ! GND VCC;)

     

     


    Sometimes it may be useful to hide the airwires of selected signals, for instance if these will later be connected through a polygon. Typically this could be supply signals, which have a lot of airwires that will never be routed explicitly and just obscure the other signals' airwires.

    To hide airwires the RATSNEST command can be given the exclamation mark ('!'), followed by a list of signals, as in

    RATSNEST ! GND VCC

    which would hide the airwires of the signals GND and VCC.
    To have the airwires displayed again just enter the RATSNEST command without the '!' character, and the list of signals:

    RATSNEST GND VCC

    This will activate the display of the airwires of the signals GND and VCC and also recalculates them. You can also recalculate the airwires (and polygons) of particular signals this way.

    The signal names may contain wildcards, and the two variants may be combined, as in

    RATSNEST D* ! ?GND VCC

    which would recalculate and display the airwires of all signals with names beginning with 'D', and hide the airwires of all the various GND signals (like AGND, DGND etc.) and the VCC signal. Note that the command is processed from left to right, so in case there is a DGND signal the example would first process it for display, but then hide its airwires.

    To make sure all airwires are displayed enter

    RATSNEST *

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • huayuliang
    0 huayuliang over 16 years ago in reply to Richard_H

    Thank you for your detailed reply.

     

    but  these command is too much for many users, especially non-English users.

     

    so I think the User-defined panel button is needed. these function can accomplish by official or user .

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 16 years ago in reply to huayuliang

    Hi,

     

    I will forward your suggestion. Thank you.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 16 years ago in reply to huayuliang

    Hi,

     

    I will forward your suggestion. Thank you.

     

    Regards,

    Richard