Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Is Auto Scroll available?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 190 subscribers
  • Views 782 views
  • Users 0 members are here
Related

Is Auto Scroll available?

e14 Contributor
e14 Contributor over 16 years ago

I've been using Eagle for 10 years and never thought about automatic scrolling until I used Alitum Designer. Now, I want this feature in Eagle. Is it already capable of doing this through a workaround?

 

Thank you. image

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Richard_H

    Interesting. I have only used the mouse wheel to zoom in and out, in effect, to pan the layout.

    I will try your suggestion. Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 16 years ago in reply to Richard_H

    Thats true - I find that there are lots of little tricks in Eagle which are great helps with productivity.

     

    Here are a few of my favourite, which I will also post as a new discussion:

     

    1. Panning - hold down the middle mouse button to pan the drawing/board. As Richard said, you can even do this while in the middle of another command, such as route, move etc.

     

    2. Zoom wheel - I used to dislike the Eagle mouse zooming, until I realised how it works. Use the scroll wheel on the mouse to zoom in/out and (this is the trick) the zoom is centered about the mouse so you can quickly move from the left to right of a schematic or board by zooming out and back in again - it's cool.

     

    3. Text entry of commands - as a true Mac GUI user I didn't understand why we had text entry - until I started using it. It is so quick and easy to do add/move/net/name/value in a quick sequence using text commands - I find I can work much faster this way than by moving the mouse to the buttons all the time. Of course you can assign commands to function keys to, but on a mac I like the default actions already on the function keys such as Exposé, Spaces and iTunes shuttle commands etc.

     

    4. Spaces (Mac only) - set up 'Spaces' to have your board in one window and schematic in another and it's so easy to swish between them (yes thats swish not switch!) the schematic slides out and the board slides in - and you can even have data sheets and the farnell website in another to spaces. If you're on a mac and have never used Spaces or Expose I highyt recommend you give it a try. Simples.

     

    -Kenny.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Richard_H
    0 Richard_H over 16 years ago

    Aaron,

     

    EAGLE does not support auto scrolling. But EAGLE's method of panning the drawing window with a middle mouse click and moving the mouse is a very convenient and quick way. You even don't have to interrupt the currently active commend for this.

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • huayuliang
    0 huayuliang over 16 years ago
    Could you  explain "Auto Scroll" in detail ?