Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum continuos routing help
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 339 views
  • Users 0 members are here
Related

continuos routing help

e14 Contributor
e14 Contributor over 15 years ago

Every time i finish a route from a connection, if i did stop in the middle of a staright line, then when i try to move the line is broken in pieces. I have to move each segment to move a full line.

How i can make that all the routes to be one segment and not many.

I was suggested to use optimize from the set menu, but it does not work in a board which is already done.

Thanks

Ion

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 15 years ago

    Hi Ion,

     

    there is the OPTIMIZE command that joins wire segments which lie in one straight line. The individual segments must be on the same layer and have the same width. This command is useful to reduce the number of objects in a drawing and to facilitate moving a complete track instead of individual segments.

     

    It seems as if this does not work in your layout. What is the routing grid you are using? Could also be an grid issue...

    As an alternative you can do a GROUP MOVE for the trace.

    If you like, you could send me an example board by private e-mail: support at cadsoft.de . So I could take a look into it.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 15 years ago

    Hi Ion,

     

    there is the OPTIMIZE command that joins wire segments which lie in one straight line. The individual segments must be on the same layer and have the same width. This command is useful to reduce the number of objects in a drawing and to facilitate moving a complete track instead of individual segments.

     

    It seems as if this does not work in your layout. What is the routing grid you are using? Could also be an grid issue...

    As an alternative you can do a GROUP MOVE for the trace.

    If you like, you could send me an example board by private e-mail: support at cadsoft.de . So I could take a look into it.

     

    Regards,

    Richard