Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How do you implement a Single Point Ground in Eagle?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 1446 views
  • Users 0 members are here
Related

How do you implement a Single Point Ground in Eagle?

ddamron
ddamron over 15 years ago

I'm involved in a circuit I'm trying to develop that requires a single point ground.

This circuit is a high current Driver, and the datasheet for the chip I'm using strongly urges the use of a single point ground.

 

Let me explain...

 

High Voltage / Current coming into the board, first hits a 100uF electrolytic to suppress spikes.

 

I need to basically separate my grounds as if they are two signals, ie one for 'logic', and the other for 'drivers'.

 

The datasheet specifies to join the two grounds at the cap.

 

Is there any way to force this by using different signals?  ie GND vs GNDA

 

Regards,

 

Dan Damron

  • Sign in to reply
  • Cancel
Parents
  • jerryb1
    0 jerryb1 over 15 years ago

    What I do is draw the schematic with separate grounds as required with different names, connect them using a resistor with zero ohms. Place that resistor where you want(at the cap). After routing is completed then you can replace the resistor with a trace or actually put in a 0 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jerryb1
    0 jerryb1 over 15 years ago

    What I do is draw the schematic with separate grounds as required with different names, connect them using a resistor with zero ohms. Place that resistor where you want(at the cap). After routing is completed then you can replace the resistor with a trace or actually put in a 0 ohm resistor.