Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Mixed manual and auto routing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1006 views
  • Users 0 members are here
  • ripup
  • manual
  • autoroute
Related

Mixed manual and auto routing

AnaLogic
AnaLogic over 15 years ago

I have a mixed-signal design requiring me to manually route traces for RF (VHF) as striplines and to do some rather careful power supply routing.  Separately, most of the rest of the design is less critical and I'd prefer to auto-route those portions.  The manual routing, including the creation of the striplines, takes hours.  This portion of the design is relatively stable, so I'd like to do the manual routing once and leave it untouched as the rest of the design evolves.

 

I'd like to be able to freely use the autorouter and ripup tools but leave the manually-routed traces alone.  I have tried to do this with various techniques such as

  • Putting the manual traces on "new" layers that the autorouter does not know about and then merging these into the real copper layers at CAM time.  This requires great care in using restrictions to keep the autorouter from using the space on the board reserved for these manual routes.  In practice, this can only be done if the manual and auto traces are on completely separate sections of the board.  They are not.  The assisted manual router also does not know about these "new" layers, so this trick requires some sort of routing using the real layers and then moving the resulting routes to the new layers.  Also, DRC does not pay attention to these new layers and I can easily create a problem that DRC misses.  I don't view this as viable.
  • Doing the manual routing normally and then saving the board and schematic files as "golden" files.  I then continue doing the auto-routing, but instead of using ripup to go back, I do some fiddling around with deleting files and reverting to the golden files.  This is clumsy because the Eagle project file tracks backup versions and does not (appear to) support this kind of file fiddling.  Such fiddling usually leads me to getting the board and the schematic out of sync or otherwies confusing Eagle.  The bigger problem is that when I have to revert, I lose any subsequent changes I'd made to the schematic.  This is not a viable approach either.

 

The real need is to be able to mark the manually routed traces in some way such that the ripup command can be instructed to ignore them.  Is there some way to define an attribute, a group, or a class that I can use with the manual routes that ripup will recognize and ignore?

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    ripup ! signal1 signal2 signal3;

     

    will ripup everything except signal[1..3]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • AnaLogic
    0 AnaLogic over 15 years ago in reply to e14 Contributor

    Chris, good suggestion.  This works for some cases but not others.  One issue is that it is unwieldy for a large number of nets.  I am using a script to issue the ripup command - this helps avoid typing mistakes and lots of rekeying.  But consider another issue that may be better illustrated with an example.  Let's say I have three nets named net1, net2 and net3.  For net1, I want to route it manually, For net2, I want it to be auto-routed.  But for net3, I want to manually route some segments and autoroute the others (such as the high- and low-current segments of a power distribution net).  Let's say I manually route net1 and selected segments of net3, then I run the autorouter.  I then want to make changes that require ripping up all but the manual routes and auto-routing again.  If I say

     

      ripup ! net1;

     

    then I will retain the manual routing of net1, but I'll lose all the manually-routed segments of net3.  That's not what I want.  If instead I try

     

      ripup ! net1 net3

     

    then I will keep both net1 and the manually-routed *AND* the auto-routed segments of net3 - this is also not what I want.  I then have to go and manually rip up the auto-routed segments of net3.  This gets impractical and error-prone with many such nets.

     

    Nevertheless, I have taken your suggestion and with some careful scripting it has helped significantly.

     

    Thank you.

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • AnaLogic
    0 AnaLogic over 15 years ago in reply to e14 Contributor

    Chris, good suggestion.  This works for some cases but not others.  One issue is that it is unwieldy for a large number of nets.  I am using a script to issue the ripup command - this helps avoid typing mistakes and lots of rekeying.  But consider another issue that may be better illustrated with an example.  Let's say I have three nets named net1, net2 and net3.  For net1, I want to route it manually, For net2, I want it to be auto-routed.  But for net3, I want to manually route some segments and autoroute the others (such as the high- and low-current segments of a power distribution net).  Let's say I manually route net1 and selected segments of net3, then I run the autorouter.  I then want to make changes that require ripping up all but the manual routes and auto-routing again.  If I say

     

      ripup ! net1;

     

    then I will retain the manual routing of net1, but I'll lose all the manually-routed segments of net3.  That's not what I want.  If instead I try

     

      ripup ! net1 net3

     

    then I will keep both net1 and the manually-routed *AND* the auto-routed segments of net3 - this is also not what I want.  I then have to go and manually rip up the auto-routed segments of net3.  This gets impractical and error-prone with many such nets.

     

    Nevertheless, I have taken your suggestion and with some careful scripting it has helped significantly.

     

    Thank you.

     

    Bob