Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum GenCAD reverses polarity of capacitors!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1277 views
  • Users 0 members are here
  • gencad
Related

GenCAD reverses polarity of capacitors!

e14 Contributor
e14 Contributor over 15 years ago

I have a problem with all three versions of gencad.ulp (including 1.23 and 1.30) where my electrolytic capacitors are reversed in the CAD file compared to the .plc  The assembly house looked at the silk screen (.plc) the first time and everything was fine.  But when I re-ordered boards assembled, they looked at the CAD files and my tantalum caps nearly caught on fire!

 

I tried to decipher the ULP script and could not find any clues as to how the polarity is determined.

 

I am willing to alter my library of packages and devices to make sure this works, but I see that I am using a package that came from one of the "standard" libraries, so I am unclear as to why there is a problem.

 

I also worry that capacitors are not the only parts with incorrect orientation.

 

Note that none of my caps are oriented other than 0, 90, 180 or 270, so this should not be related to the known problems with 45 degree or other rotations.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    It could be possible that this problem is due to the Windows software that is reading and displaying the CAD files, and not gencad.ulp itself.  I will check with my assembly shop to see what version of software they're using (it's something that they purchased a license for, so I do not have my own copy).

     

    If anyone knows of a free CAD viewer for Mac OS X or Windows XP, please let me know.  It would be nice if I could verify CAD files before sending them out for a job.  The Eagle license has been more than worth the money, but I can't quite justify spending additional money on a CAD viewer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Aegis CircuitCAM is the software that apparently reveals this error. Now, the challenge is to determine whether CircuitCAM is displaying the CAM files incorrectly, or if gencad.ulp is creating them incorrectly.

     

    Note that my circuit started out with a standard Device and Package from A/3216-18R@rcl.lbr, but when I switched to my own Device and Package I noted that the default rotation was opposite.  In order to preserve my existing layout, I had to rotate the existing pieces by 180 degrees.  I still have the positive side of the Symbol attached to the positive side of the Package, so that one-time rotation should not be visible to gencad.ulp in any way.  The whole thing makes me suspicious, though.

     

    If there are no free CAD viewers, then perhaps someone can suggest a really cheap one!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Aegis CircuitCAM is the software that apparently reveals this error. Now, the challenge is to determine whether CircuitCAM is displaying the CAM files incorrectly, or if gencad.ulp is creating them incorrectly.

     

    Note that my circuit started out with a standard Device and Package from A/3216-18R@rcl.lbr, but when I switched to my own Device and Package I noted that the default rotation was opposite.  In order to preserve my existing layout, I had to rotate the existing pieces by 180 degrees.  I still have the positive side of the Symbol attached to the positive side of the Package, so that one-time rotation should not be visible to gencad.ulp in any way.  The whole thing makes me suspicious, though.

     

    If there are no free CAD viewers, then perhaps someone can suggest a really cheap one!