Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Small remaining airwires in routes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 186 subscribers
  • Views 310 views
  • Users 0 members are here
Related

Small remaining airwires in routes

Wolfskammer04
Wolfskammer04 over 14 years ago

Hello,

 

sometimes remains a small part of an airwire in the route. Is that a problem or should I do anything to let them dissappear/solve the problem? I 've the impression that at that points the connection may be not complete. I attached a picture that show this.

 

Regards

roland

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 14 years ago

    Hi Roland,

     

    the image you attached shows a small airwire because the two wire segments are obviously not properly connected. In this case I don't see a problem, the two segments overlap so they are connected, but generally it is better to have no airwires left in the layout. After RATSNEST EAGLE should report "Nothing to do!". Then you can be sure that everything is routed.

    If there are airwires, you should use the ROUTE command in order to have it properly connected.

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 14 years ago

    Hi Roland,

     

    the image you attached shows a small airwire because the two wire segments are obviously not properly connected. In this case I don't see a problem, the two segments overlap so they are connected, but generally it is better to have no airwires left in the layout. After RATSNEST EAGLE should report "Nothing to do!". Then you can be sure that everything is routed.

    If there are airwires, you should use the ROUTE command in order to have it properly connected.

     

    Regards,
    Richard