Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Error message with standard version: 6.1.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 991 views
  • Users 0 members are here
  • -
  • board
  • routage
  • routing
Related

Error message with standard version: 6.1.0

e14 Contributor
e14 Contributor over 14 years ago

Hello I try to ask my question in english.

I have made a schématic, create package of componente this step is not so hard.... But when go on the board and i create my pcb card at my dimension  and i would like translate the compononente on the pcb ...

 

The software told me that :

 

" standard edition of eagle can't perform the requested action ! Some objects extend outside the allowed board area ."

 

 

It's possible that seize of pcb is limited  on standard edition ?

 

 

Bonjour ma question est simple peut on crée des cartes au dimenssion que lon veux sur eagles CAD  car jai un message d'erreur quand je sors de la zone de la carte  crée de base par le logiciel à l'ouverture.

 

Si oui comment augmenter la taille de cette carte  ?

Attachments:
image
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Thanks you for all this informations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 14 years ago in reply to e14 Contributor

    Hi Dave_L

     

    no I am sorry the restriction is a permanent one.

     

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    But...is it possible to disable this restriction temporarily, simply to rotate or reposition components before final assembly within the restricted area??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Richard_H

    Ok  thanks !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 14 years ago

    Hi,

     

    yes the Standard Edition of EAGLE has a limitted Board area. The maximum is 160 mm x 100 mm.

    This means that all the components have to be placed with in the coordinates range of (0 0) (160 100) [mm].

    The image tells me that you try to create a board that exceeds these limits.....

     

    Regards,

    Richard