Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Add additonal information to each part and export/print it
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 398 views
  • Users 0 members are here
Related

Add additonal information to each part and export/print it

e14 Contributor
e14 Contributor over 14 years ago

Dear all,

 

is it in Eagle possible to attach additional information like max voltage, max. current and maybe more information to each part in the schema and print or export later a list where all this information is displayed?

 

Thanks

Matthias

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    As far as I know there is no way to add additional information on a part and have it available to export into a spreadsheet or whatnot. You might be able to include the extra info on the part but you won't be able to compile all the data from multiple parts into a data sheet of datasheets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 14 years ago in reply to e14 Contributor

    Hello,

     

    yes you can.

    It is possible to add any information in the library or in the schematic/layout with the ATTRIBUTE command. There are BOM ULPs that output this additional information as well, for example bom_w_attributes.ulp.

     

    ATTRIBUTE is available since EAGLE 5.0.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 14 years ago in reply to e14 Contributor

    Hello,

     

    yes you can.

    It is possible to add any information in the library or in the schematic/layout with the ATTRIBUTE command. There are BOM ULPs that output this additional information as well, for example bom_w_attributes.ulp.

     

    ATTRIBUTE is available since EAGLE 5.0.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Richard_H

    Thanks a lot for your answers, it works perfectly.

     

    Regards

    Matthias