Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Can I use a usb wifi on my Cell Phone?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 663 views
  • Users 0 members are here
Related

Can I use a usb wifi on my Cell Phone?

e14 Contributor
e14 Contributor over 14 years ago

I have an old cell phone with no wifi. I want to be able to use wifi on it, as the data in my area costs a small fortune! The phone has a mini usb port. I was thinking and if I got a mini usb to female usb and plugged the usb wifi stick into that could I code it or modify it to work on my phone (Blackberry OS).On the pack it says that it needs windows to run, but sometimes things can work even if its don"t meet what the device needs. Also the usb wifi connector can be bought for around $20. Any and all ideas are welcome! Thank you in advance!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to GoJian

    Thanks! It was something that was on my mind and I had no clue what to do or even if it were possible. Your answer was very informative and I realize that even if this project was possible it would be way over my head. thanks anyways!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • GoJian
    0 GoJian over 14 years ago

    Hi Nathan, Good idea; however more than likely it won't work.  To be able to use usb devices, your phone must first support USB host mode - which essentially means that it must be able to supply power to the usb device.  I have never seen any Blackberry that has that capability.  Some recent Android phone has that, but you have to first root the phone and do some tricks with the linux kernel.  Then a second difficulity is to install the driver.  Most Android kernels are stripped down to save memory; so if the device is not recognized, you might have to compile your own wifi driver kernel module or switch to a different kernel.  All of these operations are quite involved...  I don't think any Blackberry OS come even close to be able to support these hacks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer