Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum "Assemblies" in Eagle?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 1107 views
  • Users 0 members are here
  • board
  • components
  • cadsoft
Related

"Assemblies" in Eagle?

nursebob
nursebob over 13 years ago

I'm aware that Eagle is not quite the same as other CAD programs such as used in architecture.  However, I'm wondering if there's a better way to make an "assembly" than what I've devised.  In other systems assemblies are a precombined set of components which can be added to a drawing.  In my case, I have some ICs I use (charge pumps in particular) where there's a set of standard components (resistors and capacitors) which use a consistent layout of the components.

I have created packages which include all the required components in an appropriate layout, and variants which allow me to control whether all the components reside on just one layer, or both top and bottom.  However, since the package is fixed, when I place it on a board, I can't deal with the sub-component separately (expected behavior).

So, is there a better way to pre-design an IC and its supporting components?  Or do I stick with what I've got?

I can live with there being no real alternative, but my solution is a bit klunky... image

 

Bob

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 13 years ago

    Hi Bob,

     

    EAGLE allows to combine any pair of consistent schematic and boards. So if you designed a schematic and routed the layout, you could save it and reuse it whenever you want to.

    Use the Edit/Import menu and select schematic/board you want to import.

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nursebob
    0 nursebob over 13 years ago in reply to Richard_H

    Richard,

     

    Thanks for the answer! image

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to nursebob

    I find assemblies annoying (to say the least) last night i had to uncheck over 5000 check boxes - so some suggestions:

    to Cadsoft:

     

    - add two entries to the 'Change' Menu "Add variant" and "Remove Variant" - last night if I could have selected all the components on 12 sheets and removed them from my new variant I would have been done in about a minute

    - some where in the docs explain how to generate a BOM for a particular assembly (took me ages to figure that one out - at the very least put something in that empty default menu like 'default assembly')

    - create a way to make a new variant based on an existing one (rather than the default)

    - finally, mixing the word s"variant" and "assembly" to mean the same thing is confusing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to nursebob

    I find assemblies annoying (to say the least) last night i had to uncheck over 5000 check boxes - so some suggestions:

    to Cadsoft:

     

    - add two entries to the 'Change' Menu "Add variant" and "Remove Variant" - last night if I could have selected all the components on 12 sheets and removed them from my new variant I would have been done in about a minute

    - some where in the docs explain how to generate a BOM for a particular assembly (took me ages to figure that one out - at the very least put something in that empty default menu like 'default assembly')

    - create a way to make a new variant based on an existing one (rather than the default)

    - finally, mixing the word s"variant" and "assembly" to mean the same thing is confusing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Hi Paul,

    you wrote:

    - add two entries to the 'Change' Menu "Add variant" and "Remove Variant" - last night if I could have selected all the components on 12 sheets and removed them from my new variant I would have been done in about a minute

    When you open the Assembly dialog you have to option to Delete the selected variant. I don't understand why you have to deselect

    a 5000 checkboxes. I'm probably missing something here.....

     

    - some where in the docs explain how to generate a BOM for a particular assembly (took me ages to figure that one out

    Okay, will do. The bom.ulp dialog has a combo box that allows to select the variant.

    - create a way to make a new variant based on an existing one (rather than the default)

    This is possible. In the assembly variants dialog, click on the New button.  You will be asked for the name of the variant and there is a Copy from.... option.

     

    Regards,

    Richard