Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum "Assemblies" in Eagle?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 1105 views
  • Users 0 members are here
  • board
  • components
  • cadsoft
Related

"Assemblies" in Eagle?

nursebob
nursebob over 13 years ago

I'm aware that Eagle is not quite the same as other CAD programs such as used in architecture.  However, I'm wondering if there's a better way to make an "assembly" than what I've devised.  In other systems assemblies are a precombined set of components which can be added to a drawing.  In my case, I have some ICs I use (charge pumps in particular) where there's a set of standard components (resistors and capacitors) which use a consistent layout of the components.

I have created packages which include all the required components in an appropriate layout, and variants which allow me to control whether all the components reside on just one layer, or both top and bottom.  However, since the package is fixed, when I place it on a board, I can't deal with the sub-component separately (expected behavior).

So, is there a better way to pre-design an IC and its supporting components?  Or do I stick with what I've got?

I can live with there being no real alternative, but my solution is a bit klunky... image

 

Bob

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    As to the first case I think you miss the point - I've laid out my board - 28 sheets, 1000s of components - now I want to make 2 variant missing roughly 4/7 and 5/7 of the components resp, one a proto build, the other a genuine manufacturing variant - the basic rule is don't stuff sheets 2 or 5-19, (and 20-22 for the 5/7 missing case, also leave out that unused power supply on page 3) I'd like to go to those schematic pages, do a select, all and say "remove these components from variant X" ... instead I have to go to the variant dialog and uncheck all those boxes ....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Hi Paul,

     

    okay i understand.....  I will forward this to our development team. Let's see what they think about it. Maybe we will improve this for the future.

     

    Reagrds,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Hi Paul,

     

    okay i understand.....  I will forward this to our development team. Let's see what they think about it. Maybe we will improve this for the future.

     

    Reagrds,

    Richard