Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Through hole pads printing solid , no holes !.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 1386 views
  • Users 0 members are here
Related

Through hole pads printing solid , no holes !.

e14 Contributor
e14 Contributor over 13 years ago

Hi All

I am new to the forum, but not Eagle; I’ve been using it for years with great effect.

My current PCB project includes some through hole parts, caps, R's and 14 pin Dip.

When printing out I end up with solid traces and pads without component pin holes.

I have tried all the option I can think of via the Display dropdown menu and print option etc.

Was using version 6.3 moved up to 6.4 but no change. I don't think I am doing anything different

to usual. What might I be missing or a point in the right direction would be most appreciated.

Regards

Steve.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I can now answer my own question.

    An aging HP laser printer that I have used for years,

    has just had its driver updated. It now fills all

    through hole IC package pads, i.e. no holes. Go figure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi I've just been scratching my head with this,

     

    I thought it was an eagle problem then noticecd if I printed as a pdf the holes were their but if i print that pdf to my HP laser it also fills the holes.

     

    I'm also using an older HP it's an "LJ4050"  I might try doing a postscript version

     

    Stuart

     

    edit :

    Yeah so I went and manualy installed the HP ps driver insted of the PCL5 driver that it had installed by default and the holes are back , whooop whoop :-) hope that helps, hope your HP is one with Post Script capability too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jackmarison93
    0 jackmarison93 over 6 years ago in reply to e14 Contributor

    Hi

    This is my first post on this forum

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jackmarison93
    0 jackmarison93 over 6 years ago in reply to e14 Contributor

    Hi

    This is my first post on this forum