Can accelerometer and gyro data be sent to a computer monitor and display as a line which moves according to the sensors
Can accelerometer and gyro data be sent to a computer monitor and display as a line which moves according to the sensors
Yes ......
(I think at least one of the Freescale accelerometer demo boards comes with just such a demo app.)
But you need to explain a bit more about what you want to do to get any more useful advice.
MK
I Am trying to connect an accelerometer, gyro, whatever to a dental drill so I can observe the position of the drills on a monitor. Save position of one and have the ability to make the second parallel to the first
Hello Richard,
What you want to do is nearly impossible (if I understand you correctly).
I think you are trying to use accelerometers and gyros to estimate the position of the drill, suppose you accelerometer can measure up to 2g (not much , easily exceeded by rapid hand movement) and has an offset error of 0.1% (very good for a low cost accelerometer), that's equivalent to an acceleration error of 0.02 m/s.
After 60 seconds the error in calculated displacement will be (0.02 * 60^2)/2 = 36m (yes thirty six meters !!).
Of course in real life you get these errors in more dimensions with additional errors from the gyros.
The reason that games use vision/ir etc to estimate position of players is that you can't do it cheaply with just accelerometers and gyros.
MK
Using vision, a few cameras would be the most accurate way to go. But it's gonna be a LOT of coding and work to get it done.
I'm not familiar wth vision/ir but can it be done with other types of sensors
I'm not familiar wth vision/ir but can it be done with other types of sensors
Using vision, a few cameras would be the most accurate way to go. But it's gonna be a LOT of coding and work to get it done.