Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Slot holes for DC jack connector in Eagle CAD
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 187 subscribers
  • Views 4712 views
  • Users 0 members are here
  • eagle_software
  • slot-hole
Related

Slot holes for DC jack connector in Eagle CAD

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I'm looking for a way to make a through hole slot instead of a drill for the DC power jack connector pins (DCJ0202 from con-jack library).

I was not successful to export the gerber file with the milling information to my board house.

Could someone send me an example or give me some advice?

Thanks

Charly


image

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi Charly,

     

    It's a common problem with these connectors. There are a couple of options. One is to draw the shape on a new layer and send it with a note to the manufacturer to explain what you want (they will mill it, so you need to let them know what diameter tool to use) or the other (simpler) method is to have a huge hole (i.e. design a custom part with a much larger pad) and accept that it will be mostly empty when you solder the part (only useful for prototypes). I just do the latter for prototypes to be honest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Hi Shabaz,

    Thank you for your quick answer. I'm interested in the first option (i.e. "draw the shape on a new layer and send it with a note to the manufacturer to explain what you want (they will mill it, so you need to let them know what diameter tool to use)".

    That might sound naive but how do I export (what job do I select) a single layer? I read somewhere that some manufacturers use layer 20.

    Also what the note to the manufacturer should contain?

    Thanks

    Charly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Hi Shabaz,

    Thank you for your quick answer. I'm interested in the first option (i.e. "draw the shape on a new layer and send it with a note to the manufacturer to explain what you want (they will mill it, so you need to let them know what diameter tool to use)".

    That might sound naive but how do I export (what job do I select) a single layer? I read somewhere that some manufacturers use layer 20.

    Also what the note to the manufacturer should contain?

    Thanks

    Charly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Richard_H
    0 Richard_H over 13 years ago in reply to e14 Contributor

    Let me add the section of the manual that deals with exactly this subject:

     

    8.13 Components with Oblong Holes


    If the board manufacturer has to mill oblong holes, you have to draw the milling contour of oblong holes in a separate layer. Usually this is layer 46, Milling.
    The milling contour for components that need oblong holes can be drawn with WIRE (and possibly ARC) with a very fine wire width near or even 0 inthe Package Editor. Take a pad that has a drill diameter which lies inside the milling contour, or SMDs, for example in Top and Bottom layer, as basis forthe oblong hole.

    In case of a multilayer board you should draw a WIRE in the used inner layers at the position of the oblong holes so that it covers

    the milling contour and leaves a kind of restring around the opening.

    Please inform your board manufacturer that they have to take care on the milling data drawn in this layer. Also tell them whether

    they should be platedt hrough or not.


    Any other cutouts in the board are drawn in the same way:
    Use a separate layer, typically layer 46, Milling, and draw the milling  contours. Tell your board manufacturer that they have to take care with  this information and make special note.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Hi Shabaz,

    I followed your instructions and it worked.image

    I ordered 3 boards today. Hopefully it'll be ok.

    Thank you for your support.

    Charly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Hi Charly,

     

    I just tried it, but I used CAM Processor and then File->Open->Job and selected gerb274x.cam, and then clicked on 'Add' to create a new tab, gave it a name (e.g. bob) and set File to %N.bob and then just selected the desired layer (I wouldn't advise 20, better to use a unique layer, otherwise it's going to be confusing if the slot is not the only thing on the layer).

    Then, the generated file (filename.bob) contained some long text string inside which I believe is the machine command for the slot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    I selected the layer when I was in the CAM processor interface but can't get the right information. I enclosed a doc file with what I did.

    Attachments:
    imageSupport Eagle.doc
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Hi Charly,

     

    The layer number doesn't matter, but best to use a unique number (e.g. 100). That way, the board outline cutting tool doesn't need to be the same as the one for the small slot you need for this part. You can just select the layer when you are in the CAM processor view, assuming your board contains a part with that layer.

     

    The note should just say "Please cut a slot based on the following filename: MYBOARD.SLOT and please use a 1mm tool to cut the slot, and please plate through-hole for the slot".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer