Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Editable "subcircuits" or similar in Eagle??
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 1479 views
  • Users 0 members are here
Related

Editable "subcircuits" or similar in Eagle??

dougmc
dougmc over 9 years ago

Greetings Eagle experts.

I've done a couple of boards in Eagle, but consider myself a novice. I do have quite a lot of experience in EDA (full custom asic) and there are some things that I feel *should* be possible in the world of PCB design, but seem difficult/impossible with Eagle. Perhaps eagle isn't the best tool for the job?

 

I have a multichannel driver design that has a repeated output stage (repeated 32 times). Obviously I'd like to design it once and step-and-repeat it. That alone seems clumsy, at best.

 

What I would really like is to have that block as some kind of "subcircuit" so that if I tweak a component value, say, or alter the layout in one block, it automatically propagates through the other copies. The intent would be to wire the subcircuits together at some other level in a hierarchy.

 

This seems obvious and very desirable (to me). Is such a thing possible? Is it possible in other PCB tools? I do this type of hierarchical design/layout in IC design all the time so it seems likely it's common in PCB design too...

 

Am I just being dense?

Doug

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    Hi Doug,

     

    Welcome to Element14!

     

    What you are wanting to do sounds completely sensible to me, it's how I would try and do things like that. In EAGLE you can do what you want to an extent but not completely. For example, you can use modules in the schematic so you can define a module once and instantiate a number of copies of each module in the schematic and they'll appear in your board. They'll have unique reference designators but not in the way you may like. Basically you get the refs as defined in the module with a prefix for each module instance. But in the layout each module instance needs to be individually placed and routed still.

     

    In V8 they now have a new design blocks feature which may help with this but I am not 100% sure as I haven't used it yet. I think it'll get there, they're going in the right direction at least, they need more work on their hierarchical design implementation still though I think, especially in the board.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougmc
    dougmc over 9 years ago in reply to rachaelp

    Hi Rachel,

     

    Thanks for the reply. I'm glad to see I'm not I'm not entirely losing my mind, but I'm very disappointed that this can't be done. For me, it just seems insane to replicate layout work again and again, and then to have to try to make sure changes are made properly to each instance.

    In particular, I'm thinking of the layout. The schematic is easier to slap together, but layout changes are tedious.

     

    Maybe PCB design doesn't call for this sort of thing terribly often, but it is something I would really like... 

     

    Do you know if any other PCB design tools have this capability? I'd rather spend the money now to get something more capable and avoid the re-learning process.

    Cheers!

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to dougmc

    Hi Doug,

     

    PCB design does call for this and the exceedingly expensive really high end tools like Altium Designer and Mentor Graprice Expidition Suite probably do this exceeding well but you will be paying an awful lot of money for these tools and they are very complex to set up and use.

     

    I think the the new design blocks feature may do a lot of what you want in Eagle so I don't think it should be out of the running. It's a brand new feature in v8 and I haven't had time to try it yet so can't give a difinitive answer.

     

    Autodesk are investing heavily into adding new features rapidly so I suspect it will be getting a lot of new functionality in the coming months so it's probably a reasonable choice if you are ok with the subscription model for licensing.

     

    Best regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougmc
    dougmc over 9 years ago in reply to rachaelp

    Hi Rachel,

    Yes, it seems like Eagle is maybe heading in (what I think is) the right direction. I will remain interested. However, it seems that it can't do real hierarchical design and the modules may just be an aid to "cut and paste" style of reuse(??).

    I'm not sure I'll bother with the free version for now. It only does 2 sheets, which doesn't really allow for testing these features. The cheap version is limited to a smallish board but might be worth playing with to see how things work.

     

    I did play around with KiCad last night. I haven't delved into the board layout yet, but the schematic editor does seem to handle proper hierarchical design. I pretty quickly got my design done with a three level hierarchy. Even if the board layout is clunky cut-and-paste, at least the schematic editor seems to do things they way I consider right.

     

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to rachaelp

    rachaelp wrote:

     

    Doug McKnight wrote:

     

    Hmm, maybe I should look at version 8 in due course. I'm not sure about the subscription model. It will depend on how much, of course, but I'm also a bit cautious of investing a lot of time in a tool in the hope it gets better...

    I think it's worth looking at the freeware version of v8.0.1 which has just been released. Have a look at the design blocks feature and see if it does what you want, I think it might but I'm not 100% sure how well it works yet.

    Ok so I have just had a look and the design blocks feature basically uses pre-saved schematic / board files which then get imported into the current schematic, adding new sheets for each copy of the block and inserting a copy of the layout into the board. So, if you wanted to tweak the block you'd need to remove and re-import the block for the design(s) you were using it in, it's not going to allow you to update one copy and all the rest automatically update unfortunately.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago in reply to rachaelp

    rachaelp wrote:

     

    Doug McKnight wrote:

     

    Hmm, maybe I should look at version 8 in due course. I'm not sure about the subscription model. It will depend on how much, of course, but I'm also a bit cautious of investing a lot of time in a tool in the hope it gets better...

    I think it's worth looking at the freeware version of v8.0.1 which has just been released. Have a look at the design blocks feature and see if it does what you want, I think it might but I'm not 100% sure how well it works yet.

    Ok so I have just had a look and the design blocks feature basically uses pre-saved schematic / board files which then get imported into the current schematic, adding new sheets for each copy of the block and inserting a copy of the layout into the board. So, if you wanted to tweak the block you'd need to remove and re-import the block for the design(s) you were using it in, it's not going to allow you to update one copy and all the rest automatically update unfortunately.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dougmc
    dougmc over 9 years ago in reply to rachaelp

    Hi Rachel,

    Yes, it seems like Eagle is maybe heading in (what I think is) the right direction. I will remain interested. However, it seems that it can't do real hierarchical design and the modules may just be an aid to "cut and paste" style of reuse(??).

    I'm not sure I'll bother with the free version for now. It only does 2 sheets, which doesn't really allow for testing these features. The cheap version is limited to a smallish board but might be worth playing with to see how things work.

     

    I did play around with KiCad last night. I haven't delved into the board layout yet, but the schematic editor does seem to handle proper hierarchical design. I pretty quickly got my design done with a three level hierarchy. Even if the board layout is clunky cut-and-paste, at least the schematic editor seems to do things they way I consider right.

     

    Doug