Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Documents Samtec CAD Library for Cadsoft EAGLE Software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 13 Aug 2012 5:40 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:44 AM
  • Views 4065 views
  • Likes 2 likes
  • Comments 7 comments
Related
Recommended

Samtec CAD Library for Cadsoft EAGLE Software

element14 provides consolidated Cadsoft EAGLE CAD libraries to reduces the efforts and time put into by our EDE customer in PCB design process while creating CAD Library for specific part in a design. The provided CAD libraries has both Symbols and Footprints (Device, Symbol & Package) information and developed as per IPC standards to meets all industrial PCB design requirements. Every CAD library has part information along with Farnell and Newark order codes which helps in creating final Bill of Materials with the suppliers order codes.


This EAGLE CAD library covers a range of Samtec connectors. This library is provided in a downloadable ZIP format which includes below files:


1. Samtec Library (.lbr) file

2. List of components in the library (PDF)

3. Readme file - Gives step by step instruction on how to import and use the library file into the Cadsoft EAGLE software.

 


 

 

Samtec SeriesDescriptionLibrary Name
TSW - S SQUARE POST HEADER Single Row SAMTEC_TSW-XXX-S-X_Batch_1.lbr
TSW - S-RA
TSW - S-RE
TSW - S-LL
TSW - D SQUARE POST HEADER Double Row SAMTEC-TSW-xxx-D_Batch_1.lbr
TSW - D-RA SQUARE POST HEADER Double  Row Right Angle SAMTEC-TSW-xxx-D-xx_Batch_1.lbr
TSW - D-LL
TSW - D-LA
TSW- Q-XX SQUARE POST HEADER Double Row with .200" (5.08mm) Between Rows SAMTEC-TSW-xxx-Q-xx_Batch_1.lbr
TSW-T SQUARE POST HEADER Triple Row SAMTEC-TSW-xxx-T-xx_Batch_1.lbr
TSW-T-LL
BBD SCREW MACHINE TERMINAL SAMTEC-BBx-ERx-SLx-SDL_Batch_1.lbr
BBS SINGLE ROW SCREW MACHINE TERMINAL STRIP
ERF8 EDGE RATE SOCKET STRIP
ERM8 EDGE RATE TERMINAL STRIP
SDL LOW PROFILE SCREW MACHINE SOCKET STRIP
SL LOW PROFILE SCREW MACHINE SOCKET STRIP
SLW LOW PROFILE SOCKET STRIP
BCS BOX CONNECTOR SOCKET STRIP SAMTEC-BCS-CES-CLx_Batch_1.lbr
CES LOW PROFILE SOCKET STRIP
CLE SURFACE MOUNT SOCKET STRIP
CLM SMT MICRO SOCKET STRIP
CLP SURFACE MOUNT MICRO SOCKET STRIP
CLT SURFACE MOUNT SOCKET STRIP
FLE SOCKET STRIP SAMTEC-FLE-Mxx-Sxx_Batch_1.lbr
MLE SMT SOCKET STRIP
MMS SOCKET STRIP
SQT SOCKET STRIP
SQW SOCKET STRIP
SSM SURFACE MOUNT SOCKET STRIP
FTE SURFACE MOUNT TERMINAL STRIP SAMTEC-HTSW-FTxx_Batch_1.lbr
FTS MICRO TERMINAL STRIP
FTSH DUAL BODY, MICRO TERMINAL STRIP
HTSW HIGH TEMP. TERMINAL STRIP
SSQ SOCKET STRIP SAMTEC-SSQ-SSW_Batch_1.lbr
SSW SOCKET STRIP
TD SCREW MACHINE TERMINAL STRIP SAMTEC-Txx_Batch_1.lbr
TLW
TS
EHF EJECTOR HEADER SAMTEC_EHF_Batch_1.lbr




image
image

 

Attachments:
imageSamtec_By_element14_Batch_1.pdf
Samtec_Library.zip
  • eagle
  • connector
  • footprint
  • library
  • cad
  • board-to-board
  • symbol
  • cadsoft
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • tschanz85
    tschanz85 over 8 years ago +1
    Hi I can not use the libraries. If i select a part of it I get en error like this "Fehler: Zeile 51966, Spalte 22: Ungültig an dieser Stelle ' ". Seems there are unallowed chars in the library files. Is…
  • sebastian.schlupp@gmail.com
    sebastian.schlupp@gmail.com over 5 years ago +1
    First of all, there are errors in almost all the files. If you scroll to the proper line column mentioned in the eagle error message, you will see (or rather not see) that there is an additional invisible…
Parents
  • sebastian.schlupp@gmail.com
    sebastian.schlupp@gmail.com over 5 years ago

    First of all, there are errors in almost all the files. If you scroll to the proper line column mentioned in the eagle error message, you will see (or rather not see) that there is an additional invisible character. Remove the characters adjacent to the position mentioned in the error report and rewrite them and the error is gone. This can also be done by copying the part which contains the error and doing a find -> replace with the same text written by hand. (there are multiple errors in multiple places so a find -> replace is the best way to go).

    Second issue is the symbols at least for the single row connectors are very poorly designed. You get a symbol which is a rectangle with half the pins on one side and half on the other even though it is a single row in reality.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sebastian.schlupp@gmail.com
    sebastian.schlupp@gmail.com over 5 years ago

    First of all, there are errors in almost all the files. If you scroll to the proper line column mentioned in the eagle error message, you will see (or rather not see) that there is an additional invisible character. Remove the characters adjacent to the position mentioned in the error report and rewrite them and the error is gone. This can also be done by copying the part which contains the error and doing a find -> replace with the same text written by hand. (there are multiple errors in multiple places so a find -> replace is the best way to go).

    Second issue is the symbols at least for the single row connectors are very poorly designed. You get a symbol which is a rectangle with half the pins on one side and half on the other even though it is a single row in reality.