3M
  • Products & Partners
  • Manufacturers
  • 3M
  • More
  • Cancel
3M
Forum Grid-Eye
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3M to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 11 subscribers
  • Views 2150 views
  • Users 0 members are here
Related

Grid-Eye

kauser
kauser over 9 years ago

Has anyone attempted to use Panasonic Grid-Eye for thermal image capturing or study of heat spreading in a load?

 

I recently attempted to study heat spreading in a cylindrical container containing water inside a microwave oven - having come over the difficulties in attempting to mount the camera.

 

Would be interesting to compare/share data....

  • Sign in to reply
  • Cancel

Top Replies

  • the48sicks
    the48sicks over 8 years ago +3
    Not used the Panasonic thermal imaging device but i have a FLiR Lepton (version 1) The more recent Lepton modules will actually report the degree rating behind each pixel but mine isnt so flashy On the…
  • shabaz
    shabaz over 8 years ago in reply to maanas.adi +2 suggested
    Hi Maanas, Unfortunately I don't know what to suggest with bluetoothctl. I didn't use bluetoothctl, and frankly I don't trust any of the tools supplied with BlueZ. I don't know what the capabilities of…
  • shabaz
    shabaz over 9 years ago +1 suggested
    Hi Kauser, I have not tried, but it sounds interesting (and feasible). Obviously there is low image resolution, but interpolation could help. Also, maybe if you repeat the test multiple times under identical…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Kauser,

     

    I have not tried, but it sounds interesting (and feasible). Obviously there is low image resolution, but interpolation could help.

    Also, maybe if you repeat the test multiple times under identical conditions you can use the datasets for looking for averaging out noise in measurements (like astronomers do in their photos). From memory the Grid-Eye resolution is 0.25 degrees C (I could be wrong, so please confirm for yourself) which could be an issue.

    If you're in a university, perhaps a math or physics department may know what manipulations you can do to the captured data to observe the heat spread. They are probably used to looking for pattern/trends in numbers, which is essentially a big part of your project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kauser
    0 kauser over 9 years ago in reply to shabaz

    Hi Shabaz,

     

     

    Thank you for the message and suggestions. I will certainly try repeating the measurements several times to see if i can get the same degree of accuracy. If it gives reasonable accuracy and repeatability than it's worth persisting with due to its ease of use - Having the camera at the end of a cable as opposed to "on a PCB" would have helped the mounting process.

     

     

    Regards,

     

     

    Kauser.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kauser
    0 kauser over 9 years ago in reply to shabaz

    Hi Shabaz,

     

     

    Thank you for the message and suggestions. I will certainly try repeating the measurements several times to see if i can get the same degree of accuracy. If it gives reasonable accuracy and repeatability than it's worth persisting with due to its ease of use - Having the camera at the end of a cable as opposed to "on a PCB" would have helped the mounting process.

     

     

    Regards,

     

     

    Kauser.