Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum remove varnish mask on a part of a track
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 90 subscribers
  • Views 1789 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

remove varnish mask on a part of a track

sdecorme
sdecorme over 7 years ago

Hi,

I would like to know if there is a solution to remove the varnish mask on a part of a track on circuit studio ?

I have not enough place to make the track at the right size so I need to solder a wire on the track.

Thanks

  • Cancel

Top Replies

  • sdecorme
    sdecorme over 7 years ago in reply to sdecorme +1
    I've followed this tuto How do I create a custom pad shape? I copy the bottom layer and I change it to bottom solder . It seems to works.
Parents
  • Fred27
    Fred27 over 7 years ago

    Would you not be better adding a surface mount pad rather than just removing the solder mask?

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • sdecorme
    sdecorme over 7 years ago in reply to Fred27

    You mean creating a pad with the form of my track !

    How can I create a pad with this form ?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • sdecorme
    sdecorme over 7 years ago in reply to sdecorme

    I've followed this tuto

    How do I create a custom pad shape?

     

    I copy the bottom layer and I change it to bottom solder . It seems to works.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • sdecorme
    sdecorme over 7 years ago in reply to sdecorme

    I've followed this tuto

    How do I create a custom pad shape?

     

    I copy the bottom layer and I change it to bottom solder . It seems to works.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • tarribred61
    tarribred61 over 7 years ago in reply to sdecorme

    Yes, you did it the correct way.  Draw your shape such as a rectangle or copy the shape from another layer on the solder mask layer (top or bottom) to open up a window on the solder mask.  Be sure not to draw on the paste mask layer or it would result in putting solder paste when they assemble.

     

    To be proper, you should make the solder mask window opening slightly larger (0.05mm to 0.1mm) than the copper you are exposing to allow for alignment of the solder mask application. In your case, it may not matter much if they are the same size.