Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Circuit Studio on Multiple monitors has issues.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 91 subscribers
  • Views 990 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Circuit Studio on Multiple monitors has issues.

lainscough_dfc
lainscough_dfc over 6 years ago

As a feedback to Altium, Using a laptop with a two screens with a second monitor has some strange behaviour when positioning Dilogs on the second screen as they jump about a lot when trying to position them.

It not really ussable.

 

Positioning the Main CircuitStudio on the second monitor is better. Just about.

Unfortunately I cannot capture this as a snap to paste here.

 

Again, there no way to feedback bugs to Altium, so this seems to be the best place. Hope that they read these when doing new releases.

 

I use 125% as Im hitting that age where eye sight starts to get worse.

 

My Display setup is:

 

image

Thanks

Lee

  • Cancel

Top Replies

  • IanJ
    IanJ over 6 years ago in reply to tarribred61 +1
    Hi all, On a 2 monitor setup on a desktop PC I see no jumping about, almost everything works ok.......the only problem I see is that dragging a Pcb from one monitor to another doesn't work (I believe it…
Parents
  • tarribred61
    tarribred61 over 6 years ago

    Hi,

     

    I also have a laptop (an older HP EliteBook) and use an additional 2 monitors (so, 3 monitors in total).  I have not seen jumpy screens that you mention.  Occasionally, a dialog box ends up off the monitors and blocks operation particularly with the layer stack manager. I wrote about this a couple of years ago (https://www.element14.com/community/message/225274/l/mystery-of-the-multiple-monitors-and-the-missing-layer-stack-manage… )

     

    This has not been fixed but we found a work around mentioned in the thread.  That said, I would suspect the issue you have is with a driver and not with CircuitStudio.  My settings are close to yours but a little bit more magnification since I have gone beyond the age of fixed focus eyesight.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • IanJ
    IanJ over 6 years ago in reply to tarribred61

    Hi all,

     

    On a 2 monitor setup on a desktop PC I see no jumping about, almost everything works ok.......the only problem I see is that dragging a Pcb from one monitor to another doesn't work (I believe it did on previous CS versions).

    I am using Win10 and a GTX1050ti and a couple of Dell 2560x1440 monitors.

     

    Ian.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • IanJ
    IanJ over 6 years ago in reply to tarribred61

    Hi all,

     

    On a 2 monitor setup on a desktop PC I see no jumping about, almost everything works ok.......the only problem I see is that dragging a Pcb from one monitor to another doesn't work (I believe it did on previous CS versions).

    I am using Win10 and a GTX1050ti and a couple of Dell 2560x1440 monitors.

     

    Ian.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • lainscough_dfc
    lainscough_dfc over 6 years ago in reply to IanJ

    OK, thanks for trying. I tried using 150% but gave the same result.

    The problem area if you select default is when you move any window, say Message to to right monotor but try to position it to the left side of the screen.

     

    I have tried with two different laptops and get the same, HP and Lenovo.

     

    OK, I can live with it.

    Thanks

    Lee

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to lainscough_dfc

    lainscough_dfc What release of Windows do you use? The build number is very useful if you can find it. Also the CS release.

    Thanks,

    Clem