Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Edit Board Shape
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 91 subscribers
  • Views 2842 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Edit Board Shape

Squintz
Squintz over 6 years ago

I have a completed board and I noticed that when I view Board Information it says one of the sides is off by just a tiny bit. So, I went to click Edit Board Shape thinking I could click on the lines and have it snap into place or possibly even manually enter the coordinates. However, when I click on Edit Board Shape I can't click anything. In fact it seems that I get stuck in that command and the only way out of it is to close the file and re-open. Am I doing something wrong?

  • Cancel

Top Replies

  • adamwebber
    adamwebber over 6 years ago +1
    What you are doing sounds funny. Maybe an installation error or some kind of glitch. Something to contact the makers of the software but good luck with that. I find that one of the easiest ways to define…
  • tarribred61
    tarribred61 over 6 years ago +1
    Yes this does seem to be messed up. Mine behaves like you describe and it may be not unique to your install. To add to the prior response, I typically define the board shape on another mechanical layer…
  • jf_vt
    jf_vt over 5 years ago +1
    I have the very same issue as the original poster Is it a bug?
Parents
  • adamwebber
    adamwebber over 6 years ago

    What you are doing sounds funny.  Maybe an installation error or some kind of glitch.  Something to contact the makers of the software but good luck with that.

     

    I find that one of the easiest ways to define a board shape is to use another layer as the outline of the board.  I use the Keep-Out layer because it is also used as the board outline for the PCB manufacturers.  Using the Keep-Out layer, draw a bunch of interconnecting lines in the shape of your board.  Make sure that they all connect.  Press Shift+S to highlight only the layer in use.  Drag a box around everything to select everything in that layer.  Then from the Board Shape menu, select 'Define from selected objects' and voila, your board is now defined. 

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • clotholecesisatropos
    clotholecesisatropos over 5 years ago in reply to adamwebber

    Hello James,

     

    The bit about the Keep Out layer seems to be excellent advice.  Like Squintz, I've tried to use Board Edit.  It seems to have a mind of its own and I end up with boards that Picasso might design.  I mutter often, "Why can't I just use the Keep Out layer?", but the CS documentation doesn't mention that, only the Board Edit functions.  I'll try your suggestion soon after I finish typing Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • clotholecesisatropos
    clotholecesisatropos over 5 years ago in reply to adamwebber

    Hello James,

     

    The bit about the Keep Out layer seems to be excellent advice.  Like Squintz, I've tried to use Board Edit.  It seems to have a mind of its own and I end up with boards that Picasso might design.  I mutter often, "Why can't I just use the Keep Out layer?", but the CS documentation doesn't mention that, only the Board Edit functions.  I'll try your suggestion soon after I finish typing Thanks.