Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Updating Components in Projects
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 3 replies
  • Subscribers 90 subscribers
  • Views 886 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Updating Components in Projects

e14 Contributor
e14 Contributor over 10 years ago

Hey,

 

Does anyone know a way to transfer updated library components on to the PCB or schematics without first removing them and then loading them again? I'm not talking about updating components from the Altium Vault but rather if you have made an integrated library and then update a component there and then want this change to show up in one of your projects.

 

S

  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1 verified
    I've been playing around with CircuitStudio and getting somewhat frustrated with it but I did find a way how to update components without needing to go through all of the deleting and adding. When you…
  • AshokRao
    0 AshokRao over 10 years ago

    Hi S A,

    AFAIK, there is no option to transfer updates from an "updated" library from SCH to PCB without removing & placing the new component again. You'll have to re-compile the library, re-place the part and then take your changes from SCH to PCB..unless somebody knows otherwise??

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to AshokRao

    Hey,

     

    If this is true then it will be a huge annoyance if you ever need to change component models at a late stage of a design. Especially if it is a commonly used component like a resistors or something that you could have hundreds.

    Deleting and placing all of them again will be a torture and you will have to do it on the schematic and PCB separately. As much as I've tried it, changes will not be carried on to the PCB as long as the footprint is already there.

    Oh fun times, CS seemed such a good option when we bought it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I've been playing around with CircuitStudio and getting somewhat frustrated with it but I did find a way how to update components without needing to go through all of the deleting and adding. When you have a PCB footprint or Schematic open there is a button "Update PCB With Current Footprint" this updates the the footprint, similarly you have "Update Schematics" Button. You also need to have the PCB or schematic open that you want to update. If you need to update pin-outs you need to first update schematic and then push the changes to PCB.

    This works but as you might know from some other posts in the forum having a integrated library open at the same time with a project can cause the software to go into and endless loop of errors, especially if you compile the library. Therefore best option is to close project when you discover that a integrated library needs updating. Then update the component library compile and then reopen the project to push the changes to the project. Then close the integrated library before the software gets angry at having both of them open.

     

    Simple, isn't it.

     

    S