Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Schematic: Re-connect unconnected wires on pin
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 90 subscribers
  • Views 847 views
  • Users 0 members are here
  • frontpage
  • circuit studio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Schematic: Re-connect unconnected wires on pin

wire67
wire67 over 10 years ago

Hi,

 

I'm trying out Circuit Studio and I am having some troubles, one of them is as follow: I'm in a situation where the wires are not connected to the pins anymore (4 dots), how can I connect them without redrawing everything as this would be very inefficient? I tried placing a manual junction but it didn't help.

This situation can be reproduced by deleting and replacing the component.

 

Thank you for your help,

Jérôme

  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    When I usually update the components then they are still connected unless I change the pin locations. Now when replacing a component then when you place it on the schematic you need to get these red crosses at the end of the pins this shows that it will reconnect to the wire. If you use a metric grid on the schematic then you can only use components that you have made on a metric grid otherwise you can run into problems aligning up pins and wires. All the components from the vault are in imperial so you can't use any of those on a metric grid without running into a lot of troubles.

     

    S

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • wire67
    0 wire67 over 10 years ago in reply to e14 Contributor

    Thx it was all imperial but you brought me to the right track:

    The pins of my custom component were not aligned to the grid, so I did for the component model and the schematic wires:

    - select all

    - tool > align > align to grid (Shift+Ctrl+D)