Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Selective thermal relief for thru holes, smt pads, vias in CircuitStudio?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 95 subscribers
  • Views 5717 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Selective thermal relief for thru holes, smt pads, vias in CircuitStudio?

nszmnsky
nszmnsky over 10 years ago

I often need to change the connection of a polygon depending on what connecting to - for instance, often want direct for vias but X on smt pads. Can this be done in CS? I don't see a way to configure rule for anything other than net, no option for setting what its connecting to.

 

Thanks

Neil

  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 10 years ago +1 suggested
    Check the design rules under Plane > Polygon Connect Style > Polygon Connect.
  • nszmnsky
    nszmnsky over 10 years ago in reply to michaelwylie +1 suggested
    I do not see an option to select different connect styles for different features. Only settings are for net and/or layer combinations. I want to not have thermal relief on vias but have them on thru holes…
Parents
  • harvie256
    0 harvie256 over 10 years ago

    The answer to this question using the built in CS tools is no.  Altium have removed some of the query stuff necessary from AD.  They made a mess of this in my opinion.

     

    However, given this is tool I bought and use, I needed to find a way.  So I manually edit rules outside of CS and re-import them, as the backend is still the same as AD and still works the same way.  See my question over at the eevblog forum for how I do it:

    http://www.eevblog.com/forum/altium/polygon-pour-connection-for-vias/

     

    As an example, below is the contents of the exported and modified .RUL file for no relief on vias, but relief on everything else:

     

    SELECTION=FALSE|LAYER=TOP|LOCKED=FALSE|POLYGONOUTLINE=FALSE|USERROUTED=TRUE|UNIONINDEX=0|RULEKIND=PolygonConnect|NETSCOPE=AnyNet|LAYERKIND=SameLayer|SCOPE1EXPRESSION=IsVia|SCOPE2EXPRESSION=All|NAME=PolygonConnect_Via|ENABLED=TRUE|PRIORITY=1|COMMENT= |UNIQUEID=YEEDPGAH|DEFINEDBYLOGICALDOCUMENT=FALSE|CONNECTSTYLE=Direct|RELIEFCONDUCTORWIDTH=10mil|RELIEFENTRIES=4|POLYGONRELIEFANGLE=90 Angle|AIRGAPWIDTH=10mil¶

    SELECTION=FALSE|LAYER=TOP|LOCKED=FALSE|POLYGONOUTLINE=FALSE|USERROUTED=TRUE|UNIONINDEX=0|RULEKIND=PolygonConnect|NETSCOPE=AnyNet|LAYERKIND=SameLayer|SCOPE1EXPRESSION=All|SCOPE2EXPRESSION=All|NAME=PolygonConnect_all|ENABLED=TRUE|PRIORITY=2|COMMENT= |UNIQUEID=IPIHNEGD|DEFINEDBYLOGICALDOCUMENT=FALSE|CONNECTSTYLE=Relief|RELIEFCONDUCTORWIDTH=10mil|RELIEFENTRIES=4|POLYGONRELIEFANGLE=45 Angle|AIRGAPWIDTH=10mil¶

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • nszmnsky
    0 nszmnsky over 10 years ago in reply to harvie256

    Thanks harvie256! IF I had a list of design rule options AND IF I wanted to manually create the rules I could accomplish what I need. I still have trouble wrapping my head around the use of rules to control PCB layout. I'm coming from NI Ultiboard where things such as reliefs, min width and spacing are Properties of the item, and each instance of the item can be individually manipulated. Want only one via direct connected? Just click on it and set the property. Want to set the relief style, spoke, and air gap of a polygon? Just click on it and set all those properties in one place. Problem is I haven't upgrade Ultiboard for a few years so have been evaluating other PCB packages to see if I should switch. I do like CS's ability to import from other PCB packages like Eagle as well as from Designer (by exporting as previous version). Of the PCB packages I've looked at, CS has the most plus's  - just not sure enough of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • nszmnsky
    0 nszmnsky over 10 years ago in reply to harvie256

    Thanks harvie256! IF I had a list of design rule options AND IF I wanted to manually create the rules I could accomplish what I need. I still have trouble wrapping my head around the use of rules to control PCB layout. I'm coming from NI Ultiboard where things such as reliefs, min width and spacing are Properties of the item, and each instance of the item can be individually manipulated. Want only one via direct connected? Just click on it and set the property. Want to set the relief style, spoke, and air gap of a polygon? Just click on it and set all those properties in one place. Problem is I haven't upgrade Ultiboard for a few years so have been evaluating other PCB packages to see if I should switch. I do like CS's ability to import from other PCB packages like Eagle as well as from Designer (by exporting as previous version). Of the PCB packages I've looked at, CS has the most plus's  - just not sure enough of them.