Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Selective thermal relief for thru holes, smt pads, vias in CircuitStudio?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 95 subscribers
  • Views 5717 views
  • Users 0 members are here
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Selective thermal relief for thru holes, smt pads, vias in CircuitStudio?

nszmnsky
nszmnsky over 10 years ago

I often need to change the connection of a polygon depending on what connecting to - for instance, often want direct for vias but X on smt pads. Can this be done in CS? I don't see a way to configure rule for anything other than net, no option for setting what its connecting to.

 

Thanks

Neil

  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 10 years ago +1 suggested
    Check the design rules under Plane > Polygon Connect Style > Polygon Connect.
  • nszmnsky
    nszmnsky over 10 years ago in reply to michaelwylie +1 suggested
    I do not see an option to select different connect styles for different features. Only settings are for net and/or layer combinations. I want to not have thermal relief on vias but have them on thru holes…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    You can make Circuit Studio connect a via to a polygon pour directly and have thermal reliefs for your other pads. It takes a bit of effort though. I made a tutorial here: http://www.eevblog.com/forum/circuit-studio/how-to-selective-thermal-relief-for-vias-and-pads/

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • adamwebber
    0 adamwebber over 9 years ago in reply to e14 Contributor

    Thank You Thank You Thank You for explaining design rules to me.  Transitioning from Altium to CircuitStudio has been a little frustrating but now that I understand CircuitStudio is Altium and I just need to use the workarounds, everything is still possible.  I love the interface of CS better than Altium but I don't like all of the items that have been removed.  This discussion has been a huge help.

     

    I used to use the command IsVia in Altium while declaring polygon connect rules and for CS I have two methods of relief-connects and direct-connects using polygon pours.

    1-Declare everything as a direct-connect unless it is a component.  Priority is key.

    2-Export the Rules, edit them and Import them back in.  Unless you know how to use Altium, this can be difficult.

     

    If someone else is looking for this, I hope that they find it.  I had difficulty searching through the forums.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • adamwebber
    0 adamwebber over 9 years ago in reply to e14 Contributor

    Thank You Thank You Thank You for explaining design rules to me.  Transitioning from Altium to CircuitStudio has been a little frustrating but now that I understand CircuitStudio is Altium and I just need to use the workarounds, everything is still possible.  I love the interface of CS better than Altium but I don't like all of the items that have been removed.  This discussion has been a huge help.

     

    I used to use the command IsVia in Altium while declaring polygon connect rules and for CS I have two methods of relief-connects and direct-connects using polygon pours.

    1-Declare everything as a direct-connect unless it is a component.  Priority is key.

    2-Export the Rules, edit them and Import them back in.  Unless you know how to use Altium, this can be difficult.

     

    If someone else is looking for this, I hope that they find it.  I had difficulty searching through the forums.