Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Polygon pour priority
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 93 subscribers
  • Views 5966 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Polygon pour priority

rjcurtis
rjcurtis over 9 years ago

In Eagle when I had overlapping Polygons I could assign a priority, so there would be a precedence in them.  It seems in Altium there is this too, but I cannot find it in Circuit Studio?

 

Basically I'd like to create a pour covering an whole layer, then have several smaller pours within that layer for specific things.  I can't use a split plane as there are also some tracks on the layer.

 

It seems this is a pretty basic requirement yet it doesn't seem to be in there as far as I can tell.

  • Cancel

Top Replies

  • rjcurtis
    rjcurtis over 9 years ago in reply to e14softwareteam +4
    OK, thanks, I can that is a way to do it. But, really, export vertices to CSV files and re-import them - how does that make this a "Professional PCB Design Tool, Ready to Pick Up and Go" without something…
  • e14softwareuk
    e14softwareuk over 9 years ago in reply to denizb +1 verified
    There is an easier way (tested in CS 1.4), just right click on the polygon > Polygon Actions > Send To Back (or Bring To Front) to reorder. You will need to re-pour once they have been reordered.
Parents
  • e14softwareteam
    0 e14softwareteam over 9 years ago

    Hi Jeremy,

     

    Sorry for the delayed response!

     

    Here is your answer from the devs:

     

    Currently CircuitStudio doesn't expose the pour order even though it is stored in the PCB file.

     

    The larger outer polygons need to be created last because newer polygons are poured last in the pouring order.

     

    To fix the board you will need to re-create the large outer polygon so that it pours after the others.

     

    Open the PCB panel and choose Polygons from the drop down list.

    Click <All Polygons> and then double click on the large polygon in the list of polygons names, e.g. TOP_GND

    Write down the settings (or take screen capture), e.g.

     

    Remove islands: 2 sq mm

    Arc approx: 0.013mm

    Necks: 0.127mm

    Name: TOP_1V2_C_1

    TopLayer

    Net: 1V2_C

    Pour over all same net objects

    remove dead copper

     

    Click the Outline Vertices tab at the top and click the Menu button > Export to CSV, name it, e.g. TOP_1V2_C_1

    Cancel out of the dialog and click on the document tab to take the focus back to the PCB document

    Press Delete to delete the polygon

     

    Press the Home > Polygon button, change the Name e.g. TOP_1V2_C_1 and draw a small simple polygon anywhere on the board

     

    Double click e.g. TOP_1V2_C_1 in the panel and ensure the correct Net is specified in teh Connect to Net setting.

    Click the Outline Vertices tab

    Menu > Import From CSV and double click on the CSV file e.g. TOP_1V2_C_1.csv

    Click back to the Graphical tab

    Ensure Is Poured is ticked and click OK

    Click Repour Now

     

    The Home > Polygon Pour > Repour All button should now repour the inner polygons before the new one you just created.

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • rjcurtis
    0 rjcurtis over 9 years ago in reply to e14softwareteam

    OK, thanks, I can that is a way to do it. 

     

    But, really, export vertices to CSV files and re-import them - how does that make this a "Professional PCB Design Tool, Ready to Pick Up and Go" without something this basic being in there?  What if I have a couple overlapping areas, that is a great way to waste a lot of time.

     

    I like CS, it's faster to create schematics and layout a board than Eagle and I prefer the interface.  But then this kind of thing and the likes of Via stitching just make me wonder how serious Altium are at pushing users toward a (horrifically priced) upgrade to Altium Designer....

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Reply
  • rjcurtis
    0 rjcurtis over 9 years ago in reply to e14softwareteam

    OK, thanks, I can that is a way to do it. 

     

    But, really, export vertices to CSV files and re-import them - how does that make this a "Professional PCB Design Tool, Ready to Pick Up and Go" without something this basic being in there?  What if I have a couple overlapping areas, that is a great way to waste a lot of time.

     

    I like CS, it's faster to create schematics and layout a board than Eagle and I prefer the interface.  But then this kind of thing and the likes of Via stitching just make me wonder how serious Altium are at pushing users toward a (horrifically priced) upgrade to Altium Designer....

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Children
  • michael_n
    0 michael_n over 9 years ago in reply to rjcurtis

    i see Atlium has problem to separate CS from AD. If they cut too many functions then CS can't be a "Professional PCB Design Tool", if they add enough useful features then they'll create their own direct competitor. I personally used AD for long time and start using CS in the last months and i see that CS is still a beta/unfinished software. If you switch from AD to CS, you will experience frustration every day image But CS has really big potential to be one of the best and most affordable PCB design software, depends on how Altium allow it to grow up...