Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Creating a board outline - where are the CAD tools
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 93 subscribers
  • Views 2280 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Creating a board outline - where are the CAD tools

cpallan
cpallan over 9 years ago

I don't see a way to create a complex board outline in Circuit Studio. There are only freehand tools, no CAD type tools for outline / mounting holes. Are there tools - am I missing something?

 

Thanks,

Charlie

  • Cancel

Top Replies

  • harvie256
    harvie256 over 9 years ago in reply to mflux_gamble +1
    Unless something has change in the latest AD release, what's in CS is the same as AD for mechanical CAD sketching (if you can even call it that.) I use Fusion360 as I qualify for their free licence as…
  • optoeng
    optoeng over 9 years ago in reply to adamwebber +1
    This method works for me, also. It is also fairly easy to 'snap-in' board outlines with the regular layout tools, although not as easy as in a CAD app. First, set your Origin at some convenient datum point…
Parents
  • awardautomation
    0 awardautomation over 9 years ago

    Besides complex shapes...  there does not seem to be any tools for simply adding mounting holes.

    I would have thought this is required in almost every design.
    Please tell me if I have missed it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • awardautomation
    0 awardautomation over 9 years ago

    Besides complex shapes...  there does not seem to be any tools for simply adding mounting holes.

    I would have thought this is required in almost every design.
    Please tell me if I have missed it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • GilchristT
    0 GilchristT over 9 years ago in reply to awardautomation

    For mounting holes, I just place a through-hole pad with the pad size set to the same as the hole size and no designator. I believe that is the most common approach but could be wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • tarribred61
    0 tarribred61 over 9 years ago in reply to awardautomation

    You can design a mounting hole as a component that is just a through hole pad.  Then add clearances and keepouts as needed (for screw heads, washers, tool access, etc).  You can build up a library of these for #4, #6, M3, M2.5, etc fasteners or for plated and non-plated mounting holes.  IPC-7351 has a naming convention for mounting holes that makes it somewhat easy to assign and then figure out what these are.

     

    Once you have a schematic library and footprint library you can put the mounting holes on the schematic and then treat them like any component in the process.  This lets you have an electrical connection to a mounting hole if you want to use it for chassis ground.