Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Can hierarchical sheets save layout time
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 92 subscribers
  • Views 1852 views
  • Users 0 members are here
  • hierarchical design
  • productivity
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Can hierarchical sheets save layout time

awardautomation
awardautomation over 9 years ago

I have just read about multi-sheet design using the hierarchical approach.
This will be great for my project which involves driving 12 small dc motors with identical circuitry.

For those who are unfamiliar, basically I will have 2 a Sheet project:

  • One will be the schematic for 1 motor, with nice current limiting features etc.
  • The other will be the parent sheet, which will contain the power supply, MCU and 12 instances of the above motor sheet.

This saves me from drawing the same motor control schematic 12 times! image

Not to mention, if I want to change something later on, I only have to do it once!

 

What I want to know is: can I push this timesaving feature into my layout design?

  i.e. can I create a fully routed layout for 1 motor, and have CS automatically implement it 12 times? 

I have looked through some of the documentation but so far have not seen a way of doing this.

  • Cancel

Top Replies

  • awardautomation
    awardautomation over 9 years ago +1 verified
    I have received feedback from CS development. While the sheet entry is big time saver for schematics, there is no automatic way to propagate this through to the layout. I did find a workaround: Create…
Parents
  • jstrautman
    0 jstrautman over 9 years ago

    I was given a live demo of the full version of Altium Designer a few years back and I remember them showing us the "Snippets" feature of Designer.  This allowed you to save small sections of schematics and layouts and I believe they could be somehow linked together to allow you to then place a schematic section and the appropriate layout for that into a new design.  But I do not believe this feature is included in Circuit Studio.  I agree this would be a big time saver!

     

    I imagine someone on the forums here has found a workaround that probably isn't quite as easy as the Altium Designer method, but will probably do much the same as you are talking about.  Perhaps it is a matter of creating a small layout project and then copying from that open project into your new one???

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • jstrautman
    0 jstrautman over 9 years ago

    I was given a live demo of the full version of Altium Designer a few years back and I remember them showing us the "Snippets" feature of Designer.  This allowed you to save small sections of schematics and layouts and I believe they could be somehow linked together to allow you to then place a schematic section and the appropriate layout for that into a new design.  But I do not believe this feature is included in Circuit Studio.  I agree this would be a big time saver!

     

    I imagine someone on the forums here has found a workaround that probably isn't quite as easy as the Altium Designer method, but will probably do much the same as you are talking about.  Perhaps it is a matter of creating a small layout project and then copying from that open project into your new one???

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • tarribred61
    0 tarribred61 over 9 years ago in reply to jstrautman

    Yes I think snippets were/are a way to do this in AD.  You can search for how to use them in the Altium Designer technical notes.  Also, in AD (as in the older Protel) you could cut and paste routing from one routed section and then easily change the net names to no name.  Then you could commit the free primitives to a new net name such as from the pads of parts.  I haven't tried this with CS yet.  What you are talking about is an advanced feature (IMHO); its just a guess, but I suspect CS has this crippled so as to get a distinction between full AD and CS.

     

    You might make a test project and try copy/paste some routing from one block to another.  I'm thinking it would result in some rule violations due to net name mismatches.  If you are lucky it might allow these to be updated to take the new net names or perhaps you can do something like select all connected copper and then update the net names.