Altium CircuitStudio
  • Products & Partners
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum How can I Duplicate a PCB Layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 9 replies
  • Answers 4 answers
  • Subscribers 89 subscribers
  • Views 4376 views
  • Users 0 members are here
  • frontpage
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

How can I Duplicate a PCB Layer?

jimku
jimku over 9 years ago

Is there any way to duplicate a pcb layer? I imported a design from PADs where the copper layers came in well but the Overlay came in as a combined Silk Screen layer and Assembly drawing. I would like to duplicate this Overlay layer and make changes to make one a Silk Screen and the other an Assembly drawing. If I use the PCB filter on the Overlay layer to select Components-All then CTRL-A to select all (I can see all is selected) then paste to a new layer (Assembly Drawing Top) nothing happens. Any suggestions?

  • Cancel
Parents
  • e14softwareuk
    0 e14softwareuk over 9 years ago

    If you are not using the component comment field then it would be possible to update these as a copy of the reference designator and place them onto their own layer. The text would be associated with the component and so would move around with it. Not as quick and easy as if you could copy and paste though.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • e14softwareuk
    0 e14softwareuk over 9 years ago

    If you are not using the component comment field then it would be possible to update these as a copy of the reference designator and place them onto their own layer. The text would be associated with the component and so would move around with it. Not as quick and easy as if you could copy and paste though.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • jimku
    0 jimku over 9 years ago in reply to e14softwareuk

    Thanks again Peter. Your first suggestion may be all that I need to get the component outlines off of the silkscreen layer. The outlines were all over the solder pads or made it too tight to put the reference designators in a good place and still be readable. I'll just leave the designators on the Top overlay layer for the silkscreen. I see when I use the managed output generator, the assembly drawing pdf does show up with the outlines that I put on the Assembly Drawing Top layer (using your suggested method) and the reference designators from the Top Overlay. That's not the case for the gerber output for the Assembly Drawing. The gerber Assembly Drawing only shows the items shown on the Assembly Drawing layer. I could probably combine the two gerbers with some gerber tool but would rather not mess with it at this time.

     

    Your suggestion for using the component comment field would also work but could get messy if I didn't remember to update the comment field if changes were made in the future. I also wondered if I could put in something like =Designator in the schematic properties comment field, but that didn't work. It would also get just as messy if I just went in and added text for the reference designators on the assembly drawing layer. So... I think I'll just move the outlines to the assembly drawing layer and keep the designators on the overlay layer and just use the pdf for the assembly drawing.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 9 years ago in reply to jimku

    I've discovered there is an option to make the component comment field a live copy of the reference designator. On the component edit the comment field to be ".Designator" (no quotes). Click the LS button, go to View Options and check Convert Special Strings.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • jimku
    0 jimku over 9 years ago in reply to e14softwareuk

    Thanks once again! I just experimented with your suggestion and it appears to work just fine. I'm not going to go back and use it on this board as I think I already have what I need with a little more clean up. It's definitely worth knowing about if I need to work on another board like this.